SDL Release Notes

Table of Contents

Introduction

This release notes provides important information that will assist you in using the SDL software package for the J784S4 family of devices. This document provides the product information and known issues that are specific to the SDL software package.

New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility

What’s New

Supported Modules

SDL support for the following modules are available:

Upgrade and Compatibility

None

Supported Devices

Fixed Defects

ID Summary
PROC_SDL-5704 RTI - Test app fail
PROC_SDL-5696 BIST Example - Main R5F1 instance failure
PROC_SDL-5693 SDL: Support for building on Windows along with caveats
PROC_SDL-5690 Unstable behavior on SDL_AM_AC_CFG_TO_AC_CFG_NON_SAFE_STOG2 instance test output
PROC_SDL-3350 Illegal boundary crossing testing.

Open Defects

ID Summary
PROC_SDL-6362 Error Injection fails for ECC Aggregator R5FSS2_0 for certain RAM ID's.
PROC_SDL-6361 Error Injection fails for ECC Aggregator R5FSS2_1 .
PROC_SDL-6360 Error Injection fails for ECC Aggregator ECC_AGGR0 for certain RAM ID's.
PROC_SDL-6359 Error Injection fails for ECC Aggregator ECC_AGGR4 for certain RAM ID's.
PROC_SDL-6356 Error Injection fails for ECC Aggregator COMPUTE_CLUSTER0_MSMC_ECC_AGGR0 for certain RAM ID's.
PROC_SDL-6346 TISCI Device ID for MAIN R52 CORE 0 and CORE 1 are reversed in PBIST configuration
PROC_SDL-6345 PBIST Main Infra 1 configurations incorrectly used for Main Infra 0
PROC_SDL-6298 Illegal boundary crossing test fails with debug mode binary.
PROC_SDL-6280 bist_example fails for pbist check of ROM for some instances.
PROC_SDL-6235 A72 Boot Fails after A72 LBIST
PROC_SDL-6174 In sdl_mcrc_test_app , return value in sdl_mcrcSemiCPU_udmaCrc API is over written.
PROC_SDL-4141 STOG test fails for PVU SRC(SDL_TOG_INSTANCE_PVU0_SRC) instance.

Migration Information

PBIST tests for compute cluster instances need the C7X image. This is due to change of MCU R5F core booting in non-secure mode, since this is a change between SDK 8.5 and SDK 8.6. PBIST example, pbist_test_app and sdl_pbist_test_app generate the multicore image by default.

Tool Chain Information