5.1. Release notes - 09_00_01

5.1.1. Features

Note

New features vs previous release are marked in bold

5.1.1.1. Hardware support

  1. J784S4 E1 EVM support

  2. Fusion1 RevC daughter card with UB960 FPDLink deserializer

  3. IMX390 2MP CSI2 image sensor + UB953 FPDLink serializer

  4. Quad Port Ethernet daughter card (for CPSW9G support)

5.1.1.2. Software features

Important

Below is a summary of key features. Refer individual SDK Components release notes for more details

5.1.1.2.1. Vision Apps (ADAS, Vision, DL demos)

  • OpenVX based demos for ADAS, Vision, deep learning applications

    • FreeRTOS or SafeRTOS on C7x, R5F and Linux/QNX on A72

    • Integrates all major PSDK RTOS and PSDK LINUX SW components like TIDL, MMALIB, PDK, OpenVX, ETHFW, OpenGL, video codec, C7x algorithms, imaging/sensors, IPC, Linux, FreeRTOS, SPL/uboot.

    • Integrates all major HW components like CSI2 camera, eDP display, UART, I2C, ethernet, SD card

  • Deep Learning demos

    • Image Classification demo

      • File based

      • Camera based

    • Standalone Semantic Segmentation application

      • File based

      • Camera based

    • Standalone Object Detection application

      • File based

      • Camera based

    • Auto valet parking (AVP) demo

      • semantic segmentation, Parking spot detect and Vehicle detect algorithms

      • 1 channel, 3 algo mode (AVP1 demo)

      • 3 channel, 3 algo mode - combined network for parking spot and vehicle detect (AVP2 demo)

      • 3 channel, 5 algo mode - combined network for parking spot and vehicle detect + Three task network for Semantic Segmentation, Motion Segmentation and Depth Estimation (AVP3 demo)

    • DKAZE-based Visual Localization application

    • Debug support for the ability to debug intermediate layer information from TIDL node

  • Surround view demos

    • 3D surround view using GPU on 4x 2MP 30fps live camera input

    • 3D surround view calibration application

  • ADAS/Vision demos

    • Dense optical flow (DOF) demo

    • Stereo disparity engine demo

    • Single and multi camera to display (CSI2RX + VISS + LDC + MSC + Display) demo

    • C7x algorithm offload demo (with DMA acceleration)

    • Multi channel codec demo utilizing CSI2RX + VISS + LDC + MSC + Display

  • OpenVX target nodes

    • image pre-processing (YUV 2 RGB) nodes for DL demos

    • image post-processing and visualization nodes for deep learning, DOF, Stereo demos

    • OpenGL nodes for surround view

  • Profiling, logging and other utility APIs

  • All included MCU tasks are split between MCU2_0 (ETHFW, VPAC0 HWA), MCU2_1 (DMPAC HWA), and MCU4_0 (VPAC1), leaving MCU3_0, MCU3_1, and MCU4_1 free on main domain

5.1.1.2.2. Platform Development Kit (PDK)

  • RTOS device drivers running on R5F, C7x

  • Supported drivers and modules

    • ENET CPSW (2G & 9G in Main domain, 2G in MCU domain), RGMII (CPSW 2G), SGMII/QSGMII (CPSW_9G), lwIP, FreeRTOS & SafeRTOS

    • CSL-FL (Chip support library)

    • GPIO

    • I2C

    • IPC (inter processor communication)

    • MMCSD with FATFS

    • OSAL

    • SBL secondary bootloader

    • SCI Client (DMSC interface)

    • SPI driver (SPI, OSPI, NAND)

    • UART

    • UDMA and DRU

    • DSS display (eDP)

    • 2xCSI2-RX camera (4 cameras per instance)

    • 2xCSI2-TX

    • 2xVPAC and DMAC (VHWA)

    • FreeRTOS Support on R5, DSPs

    • SafeRTOS Support on R5, DSPs

Refer to PDK release notes LINK for more details.

5.1.1.2.3. MCU Software (MCUSW)

  • AutoSAR 4.3.1 MCAL driver and MCU1_0 example applications running on R5F (TI Arm Clang Compiler).

  • AutoSAR MCAL driver for Adc, Can, Dio, Eth, Pwm & Wdg

5.1.1.2.4. TI Deep learning Product (TIDL) and MMALIB

  • TensorFlow Lite Runtime with Delegate API support for heterogeneous execution on ARM+C7x_MMA

  • ONNX Runtime with Execution Provider support for heterogeneous execution on ARM+C7x_MMA

  • NEO-AI-DLR support - TVM model compilation for heterogeneous execution on ARM+C7x_MMA

  • Upgraded to exercise MMA REV2 IP enhancement features - Support for hardware acceleration via on-the-fly padding of tensors - Support for asymmetric quantization for TF-Lite post training quantized models

  • TIDL deep learning inference engine library running on C7x/MMA

  • Supports Caffe, ONNX, TFlite network exchange formats

  • Supported layers: Convolution, Deconvolution, Pooling, ReLU, Elt-wise, Inner product, Soft-max, and many more

  • TIDL network import tool and graph visualizer tool

  • Post Training Quantization options for 8-bit, 16-bit and mixed precision inference

  • Support for batch processing

  • Support for auto C7x code generation with TVM

  • Refer to edgeai-tidl-tools for further details

5.1.1.2.5. FFT Library for C7x/MMA (FFTLIB)

  • C7x-only kernels

  • C7x+MMA kernels

  • Note: This is packaged as a stand-alone library component, and is not integrated into any SDK level demos

5.1.1.2.6. DSP Library for C7x/MMA (DSPLIB)

  • C7x-only kernels

  • Note: This is packaged as a stand-alone library component, and is not integrated into any SDK level demos

5.1.1.2.7. MATH Library for C7x/MMA (MATHLIB)

  • C7x-only kernels

  • Note: This is packaged as a stand-alone library component, and is not integrated into any SDK level demos

5.1.1.2.8. TI OpenVX (TIOVX)

  • OpenVX v1.1 compliant implementation with graph pipelining and user data object extension support

  • OpenVX API on A72 running Linux/QNX

  • OpenVX target kernels on C7x, R5F, A72

  • OpenVX v1.1 C6x optimized kernels recompiled for C7x

  • OpenVX nodes for

    • TIDL (C7x-MMA)

    • VISS (R5F)

    • LDC (R5F)

    • MSC (multi-scalar) (R5F)

    • Pyramid (using MSC) (R5F)

    • Dense Optical Flow (R5F)

    • Stereo Disparity Engine (R5F)

    • BLNF (bilateral noise filter) (R5F)

    • CSI2-RX camera (R5F)

    • CSI2-TX (R5F)

    • Display (eDP) (R5F)

  • OpenVX tutorials for getting started

  • PyTIOVX tools for target kernel code generation

  • Performance Analyzer tool for run time logging of OpenVX graphs

  • VISS node supports heterogeneous camera support

5.1.1.2.9. Imaging

  • IMX390 2MP sensor driver (30/60fps) with IQ tuning

  • TI Auto-exposure and auto white-balance algorithms

  • Support for UB960 broadcast mode

  • Sensor framework supports heterogeneous camera support

  • Fusion2 Board support

5.1.1.2.10. Ethernet Switch Firmware (ETHFW)

  • Ethernet firmware interface API

  • Ethernet switch firmware running on R5F for CPSW9G

  • Layer 2 switching

  • FreeRTOS and SafeRTOS for Main R5F Core 0

  • FreeRTOS and SafeRTOS for Main R5F Core 1 virtual client

  • lwIP TCP/IP stack integration

  • Remote switch configuration server

  • GUI switch configuration tool

  • Inter-VLAN routing

  • IP next header filtering

  • CPSW Proxy/Server layer for remote core integration

  • Integration with AUTOSAR Eth Virtual MAC driver

  • PTP support

  • MAC-only mode support

  • Shared memory based virtual Ethernet adapter

  • Multi-core broadcast/multicast traffic using software fan-out

  • Ethernet firmware support for QSGMII mode

  • Driver support for XAUI and USXGMII modes

  • Checksum offload support for lwIP interface

  • Scatter-gather for packet transmission

5.1.1.2.11. TI Autonomous Driving Algorithms (TIADALG)

  • Image pre-processing APIs for color plane conversion and separation YUV to RGB for DL applications (C6x optimized. recompiled for C7x)

  • Camera Pose estimation API using solve pnp technique (C6x optimized. recompiled for C7x)

  • Visual localization algorithm (C6x optimized. recompiled for C7x)

  • Structure from Motion algorithm

5.1.1.2.12. FreeRTOS

  • FreeRTOS for R5F and C7x

  • lwIP TCP/IP stack integration for R5F

5.1.1.2.13. Code Gen Tools (CGT)

  • TI Compiler, assembler, linker for R5F, C7x

  • TI LLVM (CLANG) Compiler, assembler, linker for R5F

  • GCC compiler for A72 (needs to be downloaded separately)

5.1.2. Device Support and Validation Information

SoC

Build Host (OS)

Run Target (OS)

Test Plaform

J784S4

x86_64 (Linux Ubuntu 22.04)

R5F, C7x running FreeRTOS

A72 running Linux or QNX

J784S4 EVM with daughter cards

PC emulation mode (1)

x86_64 (Linux Ubuntu 22.04)

x86_64 (Linux Ubuntu 22.04)

x86_64 (Linux Ubuntu 22.04)

(1) Requires download of addon package from mySecure Software

5.1.3. Upgrade and Compatibility

In this section, we only highlight a few significant changes in this SDK. For full list of upgrade and compatibility topics, please refer to individual components release notes SDK Components.

5.1.3.1. Enet LLD

Support for scatter-gather in packet transmission has been added starting in 08.05.00 release. This feature requires a change in Enet LLD DMA API, so applications using Enet LLD APIs need to be ported to use the updated API. Developers should refer to the porting steps documented in Enet LLD User’s Guide (LINK).

5.1.3.2. MCU Software (MCUSW)

5.1.3.2.1. Ethernet

MCAL Ethernet (MCU CPSW_2G) and Virtual MAC (virtual client for CPSW_9G) drivers have been signficantly refactored to remove most dependencies with other SDK components, such as Enet LLD and UDMA LLD. The only remaining SDK dependency is with SCI Client driver. The driver configuration has also moved to a static-oriented allocation approach for TX channel, RX channel, Ring Accs, and other resources. Please refer to the Ethernet User Guide (LINK) chapter in the MCUSW documentation for further information about Ethernet module configuration.

Additionally, MCAL Ethernet driver (MCU CPSW_2G) now has Global Time support (packet timestamping) as well as support for link time and post-build configuration, in addition to pre-compile variant already supported.

MCAL Ethernet driver is not supported in Main domain CPSW_2G (CPSW_2G).

5.1.4. Known Issues

Refer to individual SDK Components release notes for known issues in each component

5.1.5. Change Requests

ID

Head Line

Original Fix Version

New Fix Version

Components

JACINTOREQ-5018

De-scope BAM enablement on J7

PSDK_8.6

PSDK_9.1

TIOVX

JACINTOREQ-6562

Minimize delays in sensor and serdes config sequence

PSDK_9.0

PSDK_9.1

IMAGING

JACINTOREQ-6637

Multiple instance support for VPAC drivers

PSDK_9.0

PSDK_9.1

IMAGING

JACINTOREQ-6636

TIDL-RT shall support scatter max operator

PSDK_9.0

PSDK_9.1

TIDL

JACINTOREQ-6636

TIDL-RT shall list operator and constraints being generated from code

PSDK_9.0

PSDK_9.1

TIDL

JACINTOREQ-6636

TIDL library shall support performance improvements

PSDK_9.0

PSDK_9.1

TIDL

JACINTOREQ-5425

VLAN support in ETHFW

PSDK_8.6

PSDK_10.x

ETHFW

JACINTOREQ-6633

Issue of structures having members with Enum type when using same header files in QNX io-sock

PSDK_9.0

PSDK_9.1

ETHFW

JACINTOREQ-6633

CPSW stat values are not seen in remoteproc trace in linux

PSDK_9.0

PSDK_9.1

ETHFW

JACINTOREQ-5443

TISCI proc_configure API shall return success for a core that supports only signed boot

PSDK_9.0

PSDK_9.1

TIFS

JACINTOREQ-5442

TIFS shall allow the user to specify processor and host combinations for unsigned boot via board configuration

PSDK_9.0

PSDK_9.1

TIFS

JACINTOREQ-5441

TIFS for security management shall conform to the Trace Debug API

PSDK_9.0

PSDK_10.x

TIFS

JACINTOREQ-5444

SAUL5: Software Readback of Written Configuration

PSDK_9.0

PSDK_10.x

TIFS

JACINTOREQ-6631

MCAL: Safety TUV Certification delayed

PSDK_9.0

PSDK_9.1

MCAL

JACINTOREQ-6616

Weston shall support USB keyboard as HID

PSDK_9.0

PSDK_9.1

GRAPHICS

JACINTOREQ-6616

Weston shall support USB mouse as HID

PSDK_9.0

PSDK_9.1

GRAPHICS

JACINTOREQ-6616

Graphics driver shall support upto 8Kx8K textures

PSDK_9.0

PSDK_9.1

GRAPHICS

JACINTOREQ-6616

GPU should support offscreen rendering with no display dependency

PSDK_9.0

PSDK_9.1

GRAPHICS

JACINTOREQ-6616

Graphics driver shall function in offscreen mode in the absence of display driver

PSDK_9.0

PSDK_9.1

GRAPHICS

JACINTOREQ-5337

Defer EC keys + DSA signature scheme

PSDK_9.0

PSDK_9.1

TIFS

JACINTOREQ-5387

Push out QNX Safety MRs to later releases based on LTTS Phase 2 resourcing

PSDK_9.0

PSDK_9.1

QNX

JACINTOREQ-6603

PDK 9.0 Board Library/Diag Requirement Scope Change

PSDK_9.0

PSDK_9.1

PDK

JACINTOREQ-6593

MMALIB shall support high precision deconvolution

PSDK_9.0

PSDK_9.1

MMALIB

JACINTOREQ-6456

MMALIB shall support 3x3 stride 3 Row flow C7120

PSDK_9.0

PSDK_9.1

MMALIB

JACINTOREQ-6510

QoS Scope Modify CR w.r.t AEN PPR and SDK restructuring

PSDK_9.0

PSDK_9.x

ADASVISION

5.1.5.1. Errata workarounds

None

5.1.6. Additional Reports

For additional reports like test report, traceability refer [LINK] (or ${PSDK RTOS_PATH}/psdk_rtos/docs/additional_reports in package)