5.2. J784S4 SBL

5.2.1. Introduction

The Secondary Bootloader (SBL) for J784S4 initializes the execution environment for multi-core applications and this can be used to demonstrate a real world product experience. This section covers additional details including execution sequence, tools and additional flashing instructions.

The SBL is essentially a baremetal application, and it uses many components from the Processor SDK

  • <PDK>/packages/ti/build : For build infrastructure

  • <PDK>/packages/ti/csl : For initialization and SoC addresses

  • <PDK>/packages/ti/board : For board and usecase specific initialization

  • <PDK>/packages/ti/drv/spi : For reading applications from OSPI flash

  • <PDK>/packages/ti/drv/udma : For reading data from boot media using DMA

  • <PDK>/packages/ti/drv/mmcsd : For reading applications from MMC/SD/eMMC

  • <PDK>/packages/ti/fs/fatfs : For reading files from MMC/SD/eMMC

  • <PDK>/packages/ti/drv/sciclient : For communicating with DMSC sub-system

  • <PDK>/packages/ti/drv/uart : For log messages

  • <PDK>/packages/ti/osal : Primitives required by ti/drv components

The SBL is in turn used by the board framework to load and start diagnostics

Bootloader Execution Sequence

  • Power On Reset

  • ROM Bootloader (RBL)

    • Software pre-programmed in J784S4 ROM memory starts executing

    • The RBL performs platform configuration and initialization.

    • It then checks sysboot pins and chooses booting device

    • The RBL then configures PLL and clock settings for R5, and boot media like eMMC, SD/MMC, OSPI, UART, PCIe, Ethernet etc for reliable boot.

    • If no valid bootloader found on booting device, the RBL checks for next booting device, based on sysboot pins

    • It then gets image size and load address by checking the X.509 certificate that is part of the bootloader image.

    • The RBL then verifies, optionally decrypts and loads the binary to internal memory at the load address specified in the X.509 certificate.

    • Finally it resets the R5 and passes control to Secondary Bootloader(SBL) running on the R5.

  • Secondary bootloader(SBL)

    • User level secondary bootloader(SBL) begins execution from internal memory. It enables ATCM, starts PMU timers for profiling, initializes the MCU, and sets up the stack, heap and globals. It then jumps to main().

    • Board Initialization is done by calls to Board_init() API.For additional details refer Processor SDK Board Support.

    • The RAT is setup. Pin MUX and UART console are setup by calling Board_init() API. The system firmware (SYSFW or TIFS) is then loaded from the boot media into the DMSC subsystem.

    • Once the system firmware is up and running, the rest of the initialization can be done.

    • This includes optionally using Board_init() to configure PLLs, LPSCs and DDR.

    • The SBL then loads the application from the boot media. If the image is signed, the application will be copied into a user specified reserved memory, and the SBL will attempt to verify the image by calling system firmware APIs. On HS devices, the boot proceeds only if image verification passes.

    • The SBL parses application image(s) for each of the core(s) from boot media and scatter loads it to memory.

    • Once the application is loaded, the SBL communicates with the system firmware to setup the clocks for the core(s) and release it from reset.

    • The core then starts executing from application entry point.

  • Variants of SBL

SBL Configuration

Boot Media

Boot Type

Sample Application

Description

SBL MMCSD

MMCSD

Legacy

Multicore Boot Test

Boots the target using an SD card containing bootloader, sysfw and application image

BootApp RTOS

Tertiary boot loader which boots main domain cores in stages from SD card

BootApp Linux

Tertiary boot loader which boots main domain cores and Linux Kernel in stages from SD card

BootApp QNX

Tertiary boot loader which boots main domain cores and QNX in stages from SD card

SBL OSPI

OSPI NOR

Legacy

Multicore Boot Test

Boots the target using bootloader, sysfw and application image which are flashed at a particular offset in OSPI NOR

BootApp RTOS

Tertiary boot loader which boots main domain cores in stages from OSPI

BootApp Linux

Tertiary boot loader which boots main domain cores and Linux Kernel in stages from OSPI

BootApp QNX

Tertiary boot loader which boots main domain cores and QNX in stages from OSPI

SBL UART

UART

Legacy

Multicore Boot Test

A Serial connection is used for transferring the bootloader binary from PC to target board through XMODEM protocol. The bootloader on execution prompts for application image to transfer through XMODEM.

SBL CUST

CUST

Legacy

Multicore Boot Test

Flavor of OSPI SBL with custom flags. With this SBL, user can control the following things

  • DDR initialization

  • Initialization of PLLs

  • Initialization of clocks

  • Skipping MCU Reset

SBL eMMC Boot0

eMMC Boot0

Legacy

Multicore Boot Test

Boots the target using bootloader, sysfw and application images which are flashed to a particular offset to eMMC Boot0 partition

SBL eMMC UDA

eMMC UDA

Legacy

Multicore Boot Test

Boots the target using bootloader, sysfw and application images which are copied to eMMC UDA partition

SBL Boot Perf CUST

OSPI NOR

Legacy

Boot Perf Test

Flavor of OSPI SBL with custom flags.

  • Skips DDR initialization

  • Uses OCMC RAM as SBL scratch memory

  • Intializes only MCU domain to save boot time

Legacy

Early CAN Response

Flavor of OSPI SBL with custom flags.

  • Skips DDR initialization

  • Uses OCMC RAM as SBL scratch memory

  • Intializes only MCU domain to save boot time

  • User needs to enable SBL_SKIP_PINMUX_ENABLE in sbl_component.mk to save pim muxing time as well

SBL MMCSD Combined

MMCSD

Combined

Multicore Boot Test

Boots the target using an SD card containing bootloader( which contains sysfw as well) and application image

SBL OSPI Combined

OSPI NOR

Combined

Multicore Boot Test

Boots the target using bootloader(which contains sysfw as well) and application image flashed at a particulat offset in OSPI NOR

SBL Combined Boot Perf CUST

OSPI NOR

Combined

Boot Perf Test

Flavor of Combined OSPI SBL with custom flags.

  • Skips DDR initialization

  • Uses OCMC RAM as SBL scratch memory

  • Intializes only MCU domain to save boot time

SBL XIP 133/166

OSPI NOR

Legacy

XIP Boot Test

Different OSPI Configurations

SBL MMCSD HLOS

MMCSD

Legacy

combined_opt.appimage

Boots high level OS Linux using an SD card containing bootloader, sysfw and HLOS application image

combined_dev.appimage

Boots high level OS U-Boot using an SD card containing bootloader, sysfw and HLOS application image

SBL OSPI HLOS

OSPI NOR

Legacy

combined_opt.appimage

Boots high level OS Linux using bootloader, sysfw and HLOS application image which are flashed to a particular offset in OSPI NOR

combined_dev.appimage

Boots high level OS U-Boot using bootloader, sysfw and HLOS application image which are flashed to a particular offset in OSPI NOR

NOTE

  • RBL requires boot loader (SBL) to be in a special format with the binary image appended to a X.509 certificate. The certificate contains the load address, size and SHA of the bootloader image.

  • For a detailed description of ROM bootloader and more information on the image format expected by the RBL refer the initialization chapter in the J784S4 Technical Reference Manual

  • In addition to the bootloader and application, the DMSC firmware binary is also needed for the SoC to complete the system boot flow.

  • If building the combined ROM boot image, the DMSC firmware binary is part of the bootloader image itself and is not flashed separately.

  • The first 256 bytes of the ATCM are reserved by SBL for its use. The SBL initializes the ATCM with 0xFF before it uses it.

  • If the multicore application image is signed using the TI Dummy Key, instead of a degenerate key (default setting) the same binary can be used on GP and HS devices. For information on the application’s X.509 certificate format, please refer Security X509 Certificate Documentation

  • When the R5 is released from reset, it will always fetch and execute the first intruction from address 0x0.

5.2.2. Block Diagram

../_images/k3_sbl_arch_block_diag.png

5.2.3. Memory Map

../_images/k3_sbl_mem_usage.png

5.2.4. Directory structure

sbl
│
├── board
│   └── k3
│       └── sbl_main.c                                        <= define main() for SBL, board specific init
│
├── build
│   ├── makefile                                              <= makefile for the SBL component
│   ├── boot_app.mk                                           <= makefile to build BootApp examples
│   ├── sbl_boot_test.mk                                      <= Builds SBL single core tests
│   ├── sbl_multicore_boot_test.mk                            <= Builds SBL multicore boot test which uses single core tests to create multicore image
│   ├── sbl_smp_test.mk                                       <= Builds example app for using SBL lib
│   ├── sbl_mcu0_boot_perf_test.mk                            <= Builds example app for SBL performance tuning
│   ├── sbl_mcu0_boot_xip_entry.mk                            <= Builds example trampoline app to demonstrate transitioning to a XIP app from SBL
│   ├── sbl_mcu0_boot_xip_test.mk                             <= Builds example app to demonstrate XIP execution from XIP capable boot media
│   ├── sbl_img.mk                                            <= builds SBL image that is loaded and executed by ROM code
│   ├── sbl_lib.mk                                            <= Builds sbl library that other apps can link into
│   └── sbl_multicore_smp.mk                                  <= Builds multi-core image from SBL lib eg. test to demonstrate symmetric multiprocessor boot (SMP)
│
├── example
│   ├── k3MulticoreApp
│   |   ├── binary
│   │   │   └── [soc]
│   │   │       ├── sbl_boot_test_<board_name>_allcoresTestApp_release.appimage                         <= SBL loadable board specific sample apps for testing SBL boot flow on GP devices
│   │   │       ├── sbl_boot_test_<board_name>_allcoresTestApp_release.appimage.signed                  <= SBL loadable board specific signed sample apps for testing SBL boot flow on HS-SE devices
│   │   │       ├── sbl_boot_test_<board_name>_allcoresTestApp_release.appimage.hs_fs                   <= SBL loadable board specific signed sample apps for testing SBL boot flow on HS-FS devices
│   │   │       └── sbl_baremetal_boot_xip_test_<board_name>_mcu1_0TestApp_release.xer5f.bin            <= Binary image that can be eXecuted In Place on XIP capable boot media
|   │   ├── [soc]
│   │   │   ├── mcuAmplinker.lds                            <= Linker command file when TI CGT is used for Asym. Multiproc. boot
│   │   │   ├── mpuAmplinker.lds                            <= GCC linker command file (for Cortex Axx cores) for Asym. Multiproc. boot
│   │   │   ├── mcuXiplinker.lds                            <= Linker command file for XIP trampoline app
│   │   │   └── xip_entry.lds                               <= Linker command file for XIP test case
|   │   ├── mcuBootPerfLinker_small.lds                     <= TI CGT Linker command file for SBL performance tuning example (for boot with MCU domain only)
│   │   ├── mcu[core#]LockStepLinker.lds                    <= Linker command file when TI CGT is used for R5 lock-step boot
│   │   ├── mpuSmplinker.lds                                <= GCC linker command file (for Cortex Axx cores) for SMP boot
│   │   ├── xip_entry.asm                                   <= Entry point of XIP trampoline app
│   │   ├── xip_stub.c                                      <= Simple SBL test app that demonstrates transitioning to a XIP app
│   │   ├── sbl_amp_multicore.c                             <= Simple SBL test that displays UART message
│   │   ├── sbl_amp_multicore_sections.h                    <= Allows same source to be loaded to different sections for different cores.
│   │   ├── sbl_mcu_0_boot_perf_benchmark.c                 <= SBL Test to tune boot performance.
│   │   ├── sbl_multicore_a53.asm                           <= Test case entry point  for Cortex-Axx cores
│   │   ├── sbl_multicore_r5.asm                            <= Test case entry point for Cortex-R5 cores
│   │   ├── sbl_multicore_r5_sections.inc                   <= Allows same source to be loaded to different sections for different MCUs.
│   │   ├── sbl_printf.c                                    <= Lightweight UART printf function for SBL testing
│   │   ├── sbl_smp_multicore.c                             <= Simple SBL SMP test that uses SBL lib to reset MPUs
│   │   └── sbl_smp_r5.asm                                  <= Provides dummy override function for __mpu_init for SMP testcase.
│   ├── boot_app
│   │     ├── binary
│   │     │      └── [board]
│   │     │             └── [bootmedia]
│   │     │                     ├── sbl_boot_app_<bootmedia>_<*(hs)>_<board_name>_mcu1_0_freertos_TestApp_relese.appimage.*           <= BootApp image which boots main domain cores in stages
│   │     │                     ├── sbl_boot_app_<bootmedia>_linux_<*(hs)>_<board_name>_mcu1_0_freertos_TestApp_relese.appimage.*     <= BootApp image which boots main domain cores and Linux on A72 core
│   │     │                     └── sbl_boot_app_<bootmedia>_qnx_<*(hs)>_<board_name>_mcu1_0_freertos_TestApp_relese.appimage.*       <= BootApp image which boots main domain cores and QNX on A72 core
│   │     ├── boot_app_main.c
│   │     ├── boot_app_mmcsd.c
│   │     ├── boot_app_mmcsd.h
│   │     ├── boot_app_ospi.c
│   │     ├── boot_app_ospi.h
│   │     ├── boot_app_priv.h
│   │     ├── linker_r5_freertos.lds      <= linker file to build BootApp
│   │     ├── r5_mpu_freertos.c           <= MPU configurations for BootApp
│   │     ├── soc
│   │     │    └── [board]
│   │     │            ├── boot_core_defs.c
│   │     │            └── boot_core_defs.h
│   │     ├── scripts
│   │     │      └── generate_latepps.sh  <= script to generate lateapp images which are multicore images generated from sbl boot test
│   │     └── multicore_images
│   │             └── [board]
│   │                    ├── multicore_*stage1.appimage*  <= lateapp1, multicore image which boots main R5 cores in stage1
│   │                    ├── multicore_*stage2.appimage*  <= lateapp2, multicore image which boots DSP cores in stage2
│   │                    └── multicore_*stage3.appimage*  <= lateapp3, multicore image which boots A72 core in stage3
│   └── eeprom_test
│        ├── sbl_eeprom_test.c  <= Simple baremetal application which checks whether EEPROM content is properly copied to DDR or not
│        └── makefile           <= makefile to build sbl_eeprom_test
│
│
├── binary                                                        <= ROM bootable SBL images for each board/boot media
│   ├── [board]
│       └── [bootmedia]
│           └── bin
│               └── sbl_[bootmedia]_img_mcu1_0_release.tiimage
│
├── lib                                                           <= SBL lib for each boot media/board supported
│   ├── [bootmedia]
│   │   └── [board]
│   │       └── r5f
│   │           └── release
│   │               └── sbl_lib_[bootmedia].aer5f
│   └── cust
│       └── [board]
│           └── r5f
│               └── release
│                   └── sbl_lib_cust.aer5f
│
├── soc                                 <= SOC specific SBL code
│   └── k3
│       ├── [soc]
|       |   └── linker.cmd              <= Linker file used for generating ROM loadable SBL image.
│       ├── sbl_err_trap.h              <= Error loops for SBL
│       ├── sbl_init.asm                <= SBL Entry point
│       ├── sbl_misc.asm                <= SBL Assembly utility functions
│       ├── sbl_log.h                   <= SBL logging framework
│       ├── sbl_sci_client.c            <= Calls system firmware on DMSC
│       ├── sbl_sci_client.h
│       ├── sbl_slave_core_boot.c       <= Code that contains the sequence to release a core from reset
│       ├── sbl_slave_core_boot.h
│       ├── sbl_soc.c                   <= Cache Ops, PMU init, image verfication, etc & SoC specific code like RAT Init..
│       ├── sbl_soc_cfg.h               <= Abstraction layer for hiding SoC level changes from SBL
│       └── sbl_profile.h               <= SBL profiling framework
│
├── src                                 <= Common drivers used across SOCs
│   ├── mmcsd
│   ├── emmc
│   ├── hyperflash
│   ├── ospi
│   ├── qspi
│   ├── uart
│   ├── rprc                            <= RPRC image parser used by SBL
│   └── spi
│
└── tools
    ├── btoccs
    ├── byteswap
    ├── ccsutil
    ├── combined_appimage               <= Creates a "combined_*" .appimage file for booting HLOS images (e.g., ATF,U-boot,Linux)
    │   ├── bin
    │   │   └── [board]
    │   │       ├── base-board.dtb          <= Default (example) Linux DTB per platform - to be replaced with desired DTB
    │   │       ├── bl31.bin                <= Checked-in ATF image from LCPD installers of latest release
    │   │       ├── bl32.bin                <= Checked-in OPTEE image from LCPD installers of latest release
    │   │       ├── Image                   <= Checked-in Kernel image from LCPD installers of latest release
    │   │       ├── u-boot.img              <= Checked-in u-boot image from LCPD installers of latest release
    │   │       ├── u-boot-spl.bin          <= Checked-in A72 SPL image from LCPD installers of latest release
    │   │       ├── combined_opt.appimage   <= Checked-in image which boots Linux from SBL
    │   │       └── combined_dev.appimage   <= Checked-in image which boots U-Boot from SBL
    │   ├── config.mk                       <= Configuration make include file. Use this to specify images to include in combined.appimage
    │   └── makefile                        <= combined_*.appimage Makefile
    ├── BootApp_binaries
    │   ├── linux                           <= These images are used to boot Linux from BootApp
    │   │   └── [board]
    │   │       ├── atf_optee.appimage            <= Checked-in ATF OPTEE appimage
    │   │       ├── tidtb_linux.appimage          <= Checked-in dtb appimage
    │   │       └── tikernelimage_linux.appimage  <= Checked-in Linux kernel appimage
    │   └── qnx                            <= These images are used to boot QNX from BootApp
    │       └── [board]
    │            ├── atf_optee.appimage    <= Checked-in ATF OPTEE appimage
    │            └── ifs_qnx.appimage      <= Checked-in QNX appimage
    │
    ├── multicoreImageGen                 <= Stitches multiple RPRC images for different cores into a single image
    ├── out2rprc                          <= Converts .out into .rprc files, so that SBL can load non-continuous memory sections
    ├── scripts                           <= Scripts used by .out  generated by CCS projects into SBL loadable images
    │   ├── K3ImageGen.bat
    │   └── K3ImageGen.sh
    └── tiImageGen                        <= Unused for AM65xx/J721E. Image generation is handled by PDK build framework (<sdk_install_path>/pdk_*/packages/ti/build/)

5.2.5. Image Formats

SBL format:

To generate a bootable image, the SBL build uses the x509CertificateGen script to sign the sbl binary with so that the ROM Boot Loader (RBL) can parse it. The image format expected by the RBL has been described in detail in the Image Format Section of the J784S4 Technical Reference Manual

Note

For HS devices, the SBL and system firmware have to be signed with the MPK. Processor SDK sign SBL and system firmware with a TI Dummy Key on HS device. Use sbl_<bootmode>_img to boot on GP devices and sbl_<bootmode>_img_hs to boot on HS devices. The build system invokes the script <PDK>/packages/ti/build/makerules/x509CertificateGen* which inturn calls OpenSSL to create the X509 certificate.

Note

For compatibility, all signed certificates must include a software revision extension with a minimum value of 1 as ROM will use this to enforce the revision programmed into the device efuses for anti-rollback protection. This default value of 1 is set into the SDK scripts but must be incremented during the lifecycle of the device if or when the efuse value is incremented. See https://software-dl.ti.com/tisci/esd/latest/6_topic_user_guides/otp_revision.html for more details.

Note

For the combined ROM boot image, SBL and system firmware are embedded in a boot image with a single x509 certificate. ROM utilizes the x509 extension ext_boot_info to support this format. The components of this format has been described in detail in the Image Format Section of the J784S4 Technical Reference Manual

Warning

The TI Dummy Key(s) MUST be replaced by customers during production with their own Private Keys. If the TI Dummy Keys are used in a production system, the system will be open to security attacks. The path of the default (dummy) key used by the signing script for HS devices is <PDK>/packages/ti/build/makerules/k3_dev_mpk.pem

Warning

While SBL and system firmware images signed with the TI Dummy Keys will work on both GP and HS devices, the boot time will be significantly impacted on GP devices. Using SBL signed by TI Dummy Keys on GP devices is only recommended during the prototyping phase - when porting code developed on GP to HS devices.

Application image format:

Two utilities - out2rprc and multicoreImageGen are used to convert an application elf image(s) into an image loadable by the SBL. The structure of a multicore application image is provided below:

../_images/multicore_image_format.png ../_images/rprc_file_format.png

RPRC File Header Format

Offset

Binary value

0x00000000

Magic String(43525052)

0x00000004

Entry Point (Location)

0x00000008

Reserved

0x0000000C

Number of Sections

0x00000010

Version

RPRC Section Header Format

Offset

Binary value

0x00000000

Load Address

0x00000004

Reserved

0x00000008

Size

0x0000000C

Reserved

0x00000010

Reserved

Multicore boot image format

Meta Header Start

Offset

Binary value

0x00000000

Magic String (0x5254534D)

0x00000004

Number of Files

0x00000008

Device ID

0x0000000C

App Image Version

Meta Header per Core

Offset

Binary value

0x00000000

Core ID

0x00000004

Image Offset

Meta Header Core End

Offset

Binary value

0x00000000

Reserved

0x00000004

Magic String End (0x444E454D)

Signed application image format:

To convert the multicore application image into a format that can be verified, the build flow uses the x509CertificateGen script to create a x509 certificate for the app image. Images that have a x509 certificate are called signed images. Signed applications images are mandatory for HS devices, but will work also work on GP devices.

Signed images are automatically detected by the SBL and loaded into a scratch memory area specified during SBL build. The scratch memory area used by default is specified in sbl_lib.mk via the flags SBL_SCRATCH_MEM_START and SBL_SCRATCH_MEM_SIZE. The SBL_SCRATCH_MEM* options can also be specified for custom builds to override the defaults.

The SBL scratch memory is unavailable to applications during app load time, as the SBL is still active. Once the SBL transfers control to the application, this memory is available for app use - in other words SBL_SCRATCH_MEM* is available during app runtime.

For information on the application’s X.509 certificate format, please refer Security X509 Certificate Documentation

5.2.6. Building the SBL and its components

This section will cover compiling SBL for GP and HS devices. It will also show how to compile a loadable appimage file from an example application, which can be used as a reference to compile your own custom application.

5.2.6.1. Pre-requisites to Building

  • Set your environment using pdksetupenv.bat or pdksetupenv.sh located in <PDK>/packages directory. Refer to Processor SDK RTOS Building for information on setting up your build environment

NOTE

  • SBL needs openssl to build. To check if openssl is present, type the following at the linux or windows prompt.

openssl version
  • To build on Linux, you need to have mono installed.

  • Refer Build Dependencies for instructions on how to install these tools, if they are not already present on your system.

5.2.6.2. Compiling SBL for GP (General Purpose) Device

Compiling the SBL

To build all the SBL components:

cd <PDK>/packages/ti/boot/sbl/build
gmake clean all (for windows)
make clean all  (for Linux)
  • SBL image files are be located at: <PDK>/packages/ti/boot/sbl/binary/

  • SBL examples are located at <PDK>/packages/ti/boot/sbl/examples/k3MulticoreApp/binary

  • SBL lib are located at <PDK>/packages/ti/boot/sbl/lib/

Compile time options for the SBL

The SBL supports several compile time options to tweak the SBL to satisfy requirements of ease of use, boot time and size. These can be enabled or disabled by editing sbl/sbl_component.mk

  • SBL_LOG_LEVEL : Controls amount of SBL logs (on the MCU UART) and system firmware logs(on WAKEUP UART). Varies from 0(no logs) to 3 (all logs)

  • SBL_USE_DMA : Valid values are 0 (use CPU to access boot media) or 1 (use DMA to access boot media).

  • SBL_DISPLAY_PROFILE_INFO : At the end of the boot process, displays a log of timestamps at which different SBL profile points are hit. This is useful to see how much time the SBL spends in different functions. SBL_LOG_LEVEL can significantly affect performance numbers.

  • SBL_ENABLE_PLL : Dials up all the PLLs calling Board_init(). Makes it easier for applications as they no longer have to initialize the PLLs. However, enabling this significantly increases boot time and power consumption. Requires system firmware to be loaded.

  • SBL_ENABLE_CLOCKS : Enables all the module clocks by calling Board_init(). Makes it easier for applications as they no longer have to enable clocks.

  • SBL_ENABLE_DDR : Initializes the DDR. At the cost of boot time, this enables applications to run from and use DDR. SBL_ENABLE_CLOCKS and SBL_ENABLE_PLL must also be enabed for this to work. Enabling this option increases the boot time.

  • SBL_SKIP_MCU_RESET : Jumps to the MCU0 application entry point without resetting the core. Enables faster boot time. Will not change the MCU’s mode (lock-step/split). Application also inherits the MCU state as the SBL left it in.

  • SBL_ENABLE_DEV_GRP_MCU : Will cause the system firmware to only use MCU domain resources during system firmware initialization. This can be done either to support boot when the main power domain is off, or to save boot time.

  • SBL_ENABLE_HLOS_BOOT: SBL will take some extra steps to prepare certain peripherals and resources to be handed over for HLOS (e.g., Linux) control from the Cortex-A cores.

  • SBL_HLOS_OWNS_FLASH : Ensures the SBL will leave the OSPI flash in single SPI mode, so that the MAIN domain Cortex-A code (e.g., HLOS) can reset the flash and take control of it, if needed.

  • SBL_SKIP_PINMUX_ENABLE : SBL will skip any PINMUX init being done in the bootloader and expect that it will be handled by a subsequent application.

  • SBL_SKIP_LATE_INIT : SBL will skip calling the SoC Late Init functions, normally contained in SBL_SocLateInit()

  • SBL_USE_MCU_DOMAIN_ONLY : SBL will configure & boot MCU domain cores ONLY. Saves boot time when configuring & using MCU domain only (especially when testing MCU-only boot or measuring Early CAN response).

The SBL also supports a “custom” build, in addition to standard out-of-box builds. A custom build is a useful way of testing out the effect of different build options - like when optimizing for boot time, or enabling custom usecases like eXecute In Place (XIP) to reduce memory usage.

For an example of how to use such custom builds, please refer to sbl/sbl_component.mk. It shows how to specify a select list of build options while building SBL images and libs.

ROM Combined Image boot

Certain devices (J7200, J721S2, and J784S4) support a combined boot image flow. In this flow, a boot binary blob has both Secondary bootloader (SBL) and System Firmware (SYS-FW) embedded in the boot image with a single X509 certificate. ROM employs a new X509 extension called ext_boot_info. It supports multiple boot components with a single certificate as described in the “Extended Boot Info Extension” of the J784S4 Technical Reference Manual and below:

../_images/combined_rom_image_format.png

To create the combined boot image, simply build an alternate SBL bootloader target with “_combined” (GP device) or “_combined_hs” (HS device) appended to the build target name (only for MMCSD or OSPI boot modes).

SBL Build Target Examples for ROM Combined image boot:

  • GP device : To boot from SD card, use the “sbl_mmcsd_img_combined” build target. For OSPI boot mode, use “sbl_ospi_img_combined”.

  • HS device : To boot from SD card, use the “sbl_mmcsd_img_combined_hs” build target. For OSPI boot mode, use “sbl_ospi_img_combined_hs”.

Note :

  • To create the combined board configurations utilized in the boot image, use make target “sciclient_boardcfg_combined”

  • The combined boot image flow defaults to using the J7200 ES2.0 TIFS version for J7200 HS variants

  • ROM does not support the combined boot image flow for J721E

  • For HS-SE non prime devices, an additional component in ext_boot_info (SYS-FW Inner certificate) is added to the boot image

HLOS boot

The SBL now also supports booting ARM Trusted Firmware (ATF) along with either U-boot or HLOS images (e.g., Linux + DTB) on the Cortex-A cores of the device, when used together with the “combined_appimage” make facility in the SBL tools dir.

To boot the combined.appimage that is produced, simply build an alternate SBL bootloader target with “_hlos” (GP device) or “_hlos_hs” (HS device) appended to the build target name (only for MMCSD or OSPI boot modes).

SBL Build Target Examples for HLOS Boot:

  • GP device : To boot from SD card, use the “sbl_mmcsd_img_hlos” build target. For OSPI boot mode, use “sbl_ospi_img_hlos”.

  • HS device : To boot from SD card, use the “sbl_mmcsd_img_hlos_hs” build target. For OSPI boot mode, use “sbl_ospi_img_hlos_hs”.

Note :

  • base-board.dtb needs to be modified to ensure that SD card filesystem (‘rootfs’) is specified for the Linux filesystem in each case.

  • For J721E SBL initializes the SERDES and hence the same should be disabled in device tree.

  • To disable serdes : Add ‘status = “disabled”;’ for serdes0, serdes1, serdes2

SBL Startup

The SBL can specify the R5 configuration (lockstep or split) that ROM needs to use when it starts up the SBL. This info is passed to ROM as a field in the X509 certificate. The value in this field can be controlled by editing the build flag R5_STARTUP_MODE in sbl/build/sbl_img.mk

  • EFUSE_DEFAULT : SBL will run with the same R5 configuration the boot rom ran in.

  • SPLIT_MODE : ROM will switch the R5 to split mode before starting the SBL (default).

Enabling/Disabling JTAG on secure devices

JTAG access is controlled using a field in the X509 certificate.

By default, for an easy out of box experience, the Processor SDK enables debug via JTAG on High Secure devices. Leaving JTAG enabled, while making it easy for software development, creates a major security hole in production devices.

To disable/change the level of JTAG access on HS devices, update the value of the debugType field in the signing scripts build/makerules/x509template.txt (when building from windows) and build/makerules/x509CertificateGen.sh (when building from linux).

Valid values are:

  • 0 : Disable all JTAG access (most secure and most restrictive)

  • 1 : Use device defaults (most secure and most restrictive)

  • 2 : Allow debug of non-secure code, when the CPU is running in secure mode, JTAG connectivity will be lost

  • 4 : Allow debug of both secure and non-secure code (least secure and least restrictive). This is the default.

Copying EEPROM Content

  • SBL copies EEPROM content to DDR

  • By default SBL copies to 0x90000000, user can also specifies to which address EEPROM content should be copied by passing EEPROM_DATA_DDR_ADDRESS=<address> while building SBL