Vision Apps Datasheet
|
Each of the datasheets in this document are automatically generated at run-time using performance and memory statistics collection libraries running across the SoC. As such, each core may have different memories that it considers L3_MEM heap. The following table can be used to identify which physical memory is being referred to by L3_MEM heap for each core.
Core | L3_MEM Location --— |
---|---|
mpux_y (R5F cores) | OCRAM (512 KB total) (TRM calls it MSRAM16KX256E0_RAM) |
c7x_1 | MSMC (3MB total) |
c7x_2 | MSMC (3MB total) |
c7x_3 | MSMC (3MB total) |
c7x_4 | MSMC (3MB total) |