TIOVX User Guide
|
TIOVX is TI's implementation of OpenVX Standard.
TIOVX allows users to create vision and compute applications using OpenVX API. These OpenVX applications can be executed on TI SoCs like TDA2x, TDA3x and TDA4x. TIOVX is fully conformant to OpenVX v1.1 specification. TIOVX also provides optimized OpenVX kernels for C66x DSP. An extension API allows users to integrate their own natively developed custom kernels and call them using OpenVX APIs. Examples showing usage of TIOVX as part of the larger system, ex, camera input and display output are also provided as part of Processor SDK Vision.
Top level block diagram of TIOVX is shown below.
The components of this diagram are described below
TIOVX Module | Description |
---|---|
Khronos Conformance Test | OpenVX conformance test from Khronos to make sure an implementation implements OpenVX according to specification |
TI Extension Conformance Test | Additional test cases from TI to test TI extention interfaces |
OpenVX API | OpenVX API as defined by Khronos |
TIOVX API | TI extensions and additional APIs in order to efficiently use OpenVX on TI platforms |
TIOVX Framework | TI's implementation of OpenVX spec. This layer is agnostic of underlying SoC, OS platform |
TIOVX Platform | This layer binds TIOVX framework to a specific platform. Ex, Processor SDK platform for TDA4x SOCs. This layer also binds TIOVX framework to a specific OS like Linux or TI-RTOS. |
TIOVX Kernel Wrapper | Kernel wrappers allow TI and customers to integrate a natively implemented kernel into the TIOVX framework. |
Examples | These are examples which show usage of TIOVX with other system level compoenents. These are not included in TIOVX package. Users should refer to SDK for these examples. |
User Kernels / Target Kernels | User kernels is an interface to integrate user kernels on HOST CPU using standard Khronos OpenVX APIs. Target kernels is a TI specific interface to integrate user kernels on target CPU like DSP |
The following describes the contents of the package.
Folder | Desc |
---|---|
concerto | Makefile build infrastructure |
conformance_tests/kernels | Kernels added only for test purposes (to test target kernel APIs) |
conformance_tests/test_conformance | Khronos OpenVX conformance test |
conformance_tests/test_engine | |
conformance_tests/test_data | Data files used for Khronos Conformance test, TI test suite, and tutorial input data files |
conformance_tests/test_executable | Khronos OpenVX conformance test executable (PC HOST emulation mode only) |
conformance_tests/test_tiovx | Additional test cases for Khronos OpenVX APIs and TI extention APIs |
docs | User documentation |
include/VX | Khronos OpenVX interface |
include/TI | TI OpenVX extension interface |
kernels/openvx-core | OpenVX defined kernels |
kernels* | TI vendor-specific kernels, including unit test for the kernels |
source/framework | TI OpenVX implementation |
source/include | |
source/vxu | |
source/platform | TI OpenVX platform adaptation layer |
tools | OpenVX use case and kernel wrapper code generation tool |
tutorial | TI OpenVX tutorials |
utils | Helpful utilities like image readers |
out | Build generated files and executables |
lib | Pre-built dependency libraries (PC) and tiovx libraries copied from out folder at end of build |