Jacinto 7 TIDL Release Notes
Version: 08.06.00, Date: Feb 22, 2023
Contents
- Introduction
- Licensing
- What's New
- Documentation
- Upgrade and Compatibility Information
- Device Support
- Validation Information
- Fixed Issues
- Known Issues
- Change Request
- Technical Support
- Package Versioning
Introduction
This package contains Texas Instrument's Deep learning solution for J784S4 SoCs from the Jacinto 7 family
Licensing
The licensing information of this product, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. Note : Below Links would work only after installing the package
Documentation
1 | User's Guide | [HTML] |
2 | Software Manifest | [HTML] |
What's New
Here are a few of the new features supported in this release:
- Support for Scatter ND layer
- Support for ELU, Hard sigmoid as activations
- Support for Gather & Scatter Max operators
- Optimization of DDR footprint for inference of a network with multiple resolutions
- Improved performance & DDR bandwidth reduction for networks via on-the-fly padding of tensors
- Support for Open Source Runtimes
- Bug fixes and improved stability
Upgrade and Compatibility Information
NA
Device Support
Target SoC | Target Plaform | Build environment (OS) | Target environment (OS) |
J784S4 EVM | x86_64 Linux PC | x86_64 (Linux) | NA |
Validation Information
This release was built and validated using the following tools:
Dependencies (included in Processor SDK RTOS):
- ivision - 01_00
- MMALIB - 02_06_02_00
- PDK - CORE SDK 08.06.00
- C7x CGT - ti-cgt-c7000_3.1.0.LTS
Dependencies (NOT included in Processor SDK RTOS):
- GCC version 5.4.0 (In Ubuntu 18.04)
- OpenCV: 4.1.0 (for Test bench Only)
- Protobuf: 3.11.3 (for Import tool only)
- Flatbuffers : 1.12.0 (for Import tool only)
Fixed Issues
ID | Description | Module | Affected Versions | Affected Platforms |
---|---|---|---|---|
TIDL-1891 | Batch processing with a batch greater than four leads to crashes on EVM | TOOL | 08.05.00 | J784S4 |
TIDL-2888 | Network with more than 16 subgraphs cannot be run using ONNX runtime | OSRT | 08.05.00 | J784S4 |
TIDL-2899 | Model compilation results in crash if 1x1 resize layer is the only layer in the network or subgraph | OSRT | 08.05.00 | J784S4 |
TIDL-2910 | On-the-fly padding might result in a crash for certain resize layer combinations | TOOL | 08.05.00 | J784S4 |
TIDL-2943 | Tflite runtime : Channel padding layer gets delegated to C7x when not supported | OSRT | 08.05.00 | J784S4 |
Known Issues
ID | Description | Module | Reported in Release | Affected Platforms | Occurrence | Workaround in this release |
---|---|---|---|---|---|---|
TIDL-2911 | Failure of models with higher DDR needs during creation of TIDL-RT object due to limited heap allocated to C7x (Signature error message : "VX_ZONE_ERROR:[tivxAlgiVisionAllocMem:line_no] Failed to Allocate memory record record_id @ space = space_id and size = size_in_bytes !!! | COMPUTE | 08.05.00 | J784S4 | Rare | Increase the heap size for C7x by modifying memory map, refer following relative path in processor SDK to understand how to modify memory map : ${PSDK_PATH}/psdk_rtos/docs/user_guide/developer_notes_memory_map.html | TIDL-1872 | Import failure for deeplabv3 (mobilenetv2 backbone) based OD+SEG Model | COMPUTE | 08.05.00 | J784S4 | Rare | TIDL-2593 | OSRT : Softmax layer with non-flattened input gets delegated to C7X-MMA instead of ARM | OSRT | 08.05.00 | J784S4 | Rare | Introduce a flatten layer before softmax or set softmax layer in deny_list runtime option |
TIDL-2602 | TF-Lite style asymmetric quantization has partial support | COMPUTE | 08.05.00 | J784S4 | Rare | Reimport the model with a symmetric quantizationStyle |
TIDL-2604 | DRU Based weight compression results in hangs for certain weight buffer dimensions | COMPUTE | 08.05.00 | J784S4 | Rare | Reimport the model with weight compression disabled |
For latest status of the issues and any new issues found post this release, please refer TI External software Incident Report. Issues on this product can be filtered with search query as project = EXT_EP AND issuetype in (Bug, Enhancement) AND Product ~ "TI Deep Learning Library"
Change Request
ID | Description | Original Fix Version | New Fix Version |
---|---|---|---|
JACINTOREQ-5398 | TIDL: Descope of 8.6 Requirements related to improving allow-listing, preprocessing and Transpose Layer | 08.06.00 | 09.00.00 |
Technical Support
For technical support, please post your questions on TI E2E Forum for Processors.
For additional assistance, contact local TI Field Application Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]
. The table below provides a descriptive reference regarding package version numbering.
Digit | Meaning | Description |
---|---|---|
1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale