Vision Apps Datasheet
Vision Apps Datasheet
  1. Basic Demos Datasheets
  2. DL Demos Datasheets
  3. SRV Demos Datasheets

Legend

Each of the datasheets in this document are automatically generated at run-time using performance and memory statistics collection libraries running across the SoC.

Each core may have different memories that it considers L3_MEM heap. The following table can be used to identify which physical memory is being referred to by L3_MEM heap for each core.

Core L3_MEM Location --—
MCU2_0 OCRAM (256 KB)
MCU2_1 OCRAM (256 KB)
MCU4_0 OCRAM (512 KB)
c7x_1 MSMC (3MB total)
c7x_2 MSMC (3MB total)
c7x_3 MSMC (3MB total)

Additionally, each core is using a default frequency which is used out of box and was the frequency used when generating the performance datasheets.

Core Frequency --------—
R5F Cores 1 GHz
C66 Cores 1.35 GHz
C7X Core 1 GHz
VPAC 650 MHz
DMPAC 520 MHz