Vision Apps User Guide
Stereo Disparity Application

Introduction

This application shows a demo of the TI Stereo Disparity Engine (SDE) hardware accelerator (HWA). The demo takes as input a sequence of input 8b or 16b gray scale left+right pair images in .bmp file format for 8b and raw .bin file format for 16b. Each pair of frames is run through Stereo Disparity OpenVX node. The stereo disparity map computed by SDE node are mapped based on a color palatte and output to files in .bmp format.

Supported plaforms

Platform Linux x86_64 Linux+RTOS mode QNX+RTOS mode SoC
Support YES YES YES J721e / J721S2 / J784S4 / J742S2 / J722S

Data flow

Note: On J722S, the algorithms running on C66_1 and C66_2 have been recompiled and are running on the second C7X.

vx_app_stereo_data_flow.png

Steps to run the application on J7 EVM

  1. Build the application and related libraries as mentioned in Build Instructions for Linux+RTOS mode
  2. A sample "app_stereo.cfg" for Stereo Depth with 8b input is provided under "/opt/vision_apps/" on the rootfs partition. Update paths and other fields if necessary.
  3. A sample "app_stereo_16bit.cfg" for Stereo Depth with 16b input is provided under "/opt/vision_apps/" on the rootfs partition. Update paths and other fields if necessary.
  4. For 8b input, run the app as shown below
    cd /opt/vision_apps
    source ./vision_apps_init.sh
    ./run_app_stereo.sh
  5. For 16b input, run the app as shown below
    cd /opt/vision_apps
    source ./vision_apps_init.sh
    ./run_app_stereo_16bit.sh
  6. Output will be sent to display.

Steps to run the application on PC Linux x86_64

  1. Build the application and related libraries as mentioned in Build Instructions for PC emulation mode
  2. A sample "app.cfg" for Stereo Depth with 8b input is provided under "${PSDKR_PATH}/vision_apps/apps/basic_demos/app_stereo/config" folder.Update paths and other fields if necessary.
  3. A sample "app_16bit.cfg" for Stereo Depth with 16b input is provided under "${PSDKR_PATH}/vision_apps/apps/basic_demos/app_stereo/config" folder.Update paths and other fields if necessary.
  4. For 8b input, run the app as shown below
    cd ${PSDKR_PATH}/vision_apps/out/PC/x86_64/LINUX/$PROFILE/
    ./vx_app_stereo_depth --cfg ${PSDKR_PATH}/vision_apps/apps/basic_demos/app_stereo/config/app.cfg
  5. For 16b input, run the app as shown below
    cd ${PSDKR_PATH}/vision_apps/out/PC/x86_64/LINUX/$PROFILE/
    ./vx_app_stereo_depth --cfg ${PSDKR_PATH}/vision_apps/apps/basic_demos/app_stereo/config/app_16bit.cfg
  6. Output will be generated as .bmp files in the "output_file_path" folder specified in app.cfg or app_16bit.cfg.
  7. View the output images in any image viewer

Sample Output

Shown below is a example input and its corresponding output

vx_app_stereo_left_in.png
Left Input
vx_app_stereo_right_in.png
Right Input
vx_app_stereo_disparity_out.png
Output Stereo Disparity Map
vx_app_stereo_histo_out.png
Output Disparity Histogram Map

Shown below is a sample display on J7 EVM

vx_app_stereo_evm_display.jpg