TISP User Guide
TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut > Class Template Reference

Detailed Description

template<typename dTypeIn, typename dTypeOut>
class TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut >

Provides the supernode style when input data is transferred in 2D form and output is transferred out in 2D form.

Definition at line 138 of file TISP_superNode.hpp.

Inherits TISP::SuperNode::superNode.

Public Member Functions

 i2d_to_o2d (std::unique_ptr< opVec > &&_myOpVec, dTypeIn *_pIn, dTypeOut *_pOut, dTypeIn *_pInBlock, dTypeOut *_pOutBlock, size_t _width, size_t _height, size_t _blockWidth, size_t _blockHeight, size_t _inPitch, size_t _outPitch, size_t _numChannels)
 Supernode constructor to create a 2D input to 2D output DMA supernode. More...
 
void exec ()
 [supernode example] More...
 
- Public Member Functions inherited from TISP::SuperNode::superNode
void execDefault (std::unique_ptr< opVec > &myOpVec)
 This function executes a given supernode. It contains the boiler plate template for block-based DMA and compute flow. The function calls the execute::graph function which in turn executes the correct compute flow. For data movement, appropriate APIs are called around the execute::graph function. Typical execute case of most superNodes variants (derived classes) More...
 
virtual ~superNode ()
 

Private Attributes

std::unique_ptr< opVec > myOpVec
 
DmaUtilsAutoInc3d_TransferDim transferDimIn
 
DmaUtilsAutoInc3d_TransferDim transferDimOut
 
dTypeIn * pIn
 
dTypeIn * pInBlock
 
dTypeOut * pOut
 
dTypeOut * pOutBlock
 

Additional Inherited Members

- Static Public Member Functions inherited from TISP::SuperNode::superNode
static Udma_DrvHandle setUdmaDrvHandle (Udma_DrvObjectInt &udmaDrvObj)
 
- Protected Member Functions inherited from TISP::SuperNode::superNode
 superNode (size_t _numChannels, size_t _numInChannels, size_t _numOutChannels)
 Supernode constructor that is called to create the supernode with appropriate parameters. Typically, used by classes derived from the superNode as part of their constructor c. More...
 
- Protected Attributes inherited from TISP::SuperNode::superNode
int32_t chIdIn [TISP_MAX_DMA_CHANNEL_SUPER_NODE]
 
int32_t chIdOut [TISP_MAX_DMA_CHANNEL_SUPER_NODE]
 
uint8_t * dmaUtilsContext
 
uint8_t * pTrMemCh [TISP_MAX_DMA_CHANNEL_SUPER_NODE]
 

Constructor & Destructor Documentation

◆ i2d_to_o2d()

template<typename dTypeIn , typename dTypeOut >
i2d_to_o2d::i2d_to_o2d ( std::unique_ptr< opVec > &&  _myOpVec,
dTypeIn *  _pIn,
dTypeOut *  _pOut,
dTypeIn *  _pInBlock,
dTypeOut *  _pOutBlock,
size_t  _width,
size_t  _height,
size_t  _blockWidth,
size_t  _blockHeight,
size_t  _inPitch,
size_t  _outPitch,
size_t  _numChannels 
)

Supernode constructor to create a 2D input to 2D output DMA supernode.

[supernode example]

Parameters
[in]&_myOpVec: Operator vector with list of nodes to be executed inside the supernode
[in]*_pIn: Input pointer in DDR space
[out]*_pOut: Output pointer in DDR space
[in]*_pInBlock: Input pointer in L2 space
[out]*_pOutBlock: Output pointer in L2 space
[in]_width: Width of 2D block in DDR
[in]_height: height of 2D block in DDR
[in]_blockWidth: Width of 2D block in L2
[in]_blockHeight: Height of 2D block in L2
[in]_inPitch: Input pitch in DDR
[in]_outPitch: Output pitch in DDR
[in]_numChannels: Total number of DMA channels to be used by the supernode (always 2)

Definition at line 14 of file TISP_i2d_to_o2d.cpp.

Member Function Documentation

◆ exec()

template<typename dTypeIn , typename dTypeOut >
void i2d_to_o2d::exec
virtual

[supernode example]

Implements TISP::SuperNode::superNode.

Definition at line 59 of file TISP_i2d_to_o2d.cpp.

Field Documentation

◆ myOpVec

template<typename dTypeIn , typename dTypeOut >
std::unique_ptr<opVec> TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut >::myOpVec
private

Definition at line 141 of file TISP_superNode.hpp.

◆ transferDimIn

template<typename dTypeIn , typename dTypeOut >
DmaUtilsAutoInc3d_TransferDim TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut >::transferDimIn
private

Structure to hold transfer properties of input DMA channel

Definition at line 142 of file TISP_superNode.hpp.

◆ transferDimOut

template<typename dTypeIn , typename dTypeOut >
DmaUtilsAutoInc3d_TransferDim TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut >::transferDimOut
private

Structure to hold transfer properties of output DMA channel

Definition at line 143 of file TISP_superNode.hpp.

◆ pIn

template<typename dTypeIn , typename dTypeOut >
dTypeIn* TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut >::pIn
private

Definition at line 145 of file TISP_superNode.hpp.

◆ pInBlock

template<typename dTypeIn , typename dTypeOut >
dTypeIn* TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut >::pInBlock
private

Definition at line 146 of file TISP_superNode.hpp.

◆ pOut

template<typename dTypeIn , typename dTypeOut >
dTypeOut* TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut >::pOut
private

Definition at line 147 of file TISP_superNode.hpp.

◆ pOutBlock

template<typename dTypeIn , typename dTypeOut >
dTypeOut* TISP::SuperNode::i2d_to_o2d< dTypeIn, dTypeOut >::pOutBlock
private

Definition at line 148 of file TISP_superNode.hpp.