MMALIB Release Notes
Version: 11.02.01
Contents
- Introduction
- Licensing
- Getting Started
- Documentation
- What's New
- Upgrade and Compatibility Information
- Device Support
- Validation Information
- Fixed Issues
- Deprecation
- Known Issues
- Technical Support
- Package Versioning
Introduction
The MMALIB package consists of the Texas Instruments optimized kernels for CNN, DSP and LINALG algorithms.
Licensing
The licensing information of this library and a complete manifest along with export control information is detailed here [HTML].
Getting Started
The MMALIB User Guide [USER_GUIDE] provides the documentation and references necessary to begin development on TI's platforms.
Documentation
Refer to following documentation for further details:
| MMALIB User Guide | Build instructions, API Guide | [USER_GUIDE] |
| Software Manifest | Licenses, terms of use | [HTML] |
What's New
Here are the new features supported in this release:
- [MMALIB-1410] Matrix-matrix-multiply Bias optimizations when scale shift and bias are constant
- [MMALIB-1421] Matrix-matrix-multiply Bias optimizations to leverage subpaneling of matrix multiplies
- [MMALIB-1394] Tensor convert support for INT32/UINT32 inputs and outputs
Upgrade and Compatibility Information
| File | Change description | User application change required | User application recompile required |
Device Support
| SoC | Host (OS) | Target (OS) | Test Platform |
| C7x, MMA | No OS | No OS |
Validation Information
This release was built and validated using the following tools:
Build Tools (NOT included in MMALIB):
- C7x CGT C7000-CGT-5.0.0 LTS
Fixed Issues
- [MMALIB-2094] matMulBias: performance degradation observed in 2 < 2 < MMA_SIZE cases
- [MMALIB-1822] Tensor Convert: If a NULL bias value is provided, a crash can occur
Known Issues
- [MMALIB-571] MMALIB_CNN_convolveBias_row_ixX_ixX_oxX_exec_cn: May produce wrong last row when padBottom = 1
- [MMALIB-612] MMALIB_CNN_pixelShuffle_row_ixX_ixX_oxX: Divergent behaviour between NatC and CI mode when execInArgs set
- [MMALIB-632] MMALIB_CNN_convolve_col_smallNo_ixX_ixX_oxX: add checkParams case for checking space allocated for virtual group to make an even number of groups when stride == 2
- [MMALIB-986] MMALIB_CNN_pixelShuffle_row_ixX_ixX_oxX: Code regarding MBlocksFlag = 1 is unreachable in Nat C given restriction that subMChannels must equal No
- [MMALIB-1324] [MMALIB_CNN_fullyConnectedBias_ixX_ixX_oxX] Missing checkParams on input/output geometries
- [MMALIB-1558] Tensor convert stride y value not considered within checkParams against dim_x
Deprecation
The following functions have been moved to the FFTLIB package
- MMALIB_FFT_dftSmall_ixX_cxX_oxX
- MMALIB_FFT_dftLarge_ixX_cxX_oxX
- MMALIB_FFT_highRadixDecompositions_ixX_cxX_oxX
- MMALIB_FFT_fft_ixX_cxX_oxX
- MMALIB_fft1dBatched_i16sc_c16sc_o16sc [C7x only]
- MMALIB_fft1dBatched_i32fc_c32fc_o32fc [C7x only]
- MMALIB_fft1d_i16sc_c16sc_o16sc [C7x only]
- MMALIB_fft1d_i32fc_c32fc_o32fc [C7x only]
Technical Support
For technical support, please post your questions on TI E2E Forum for Automotive ADAS SoCs.
For additional assistance, contact your local TI Field Applications Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.
| Digit | Meaning | Description |
|---|---|---|
| 1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
| 2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
| 3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
| 4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
Copyright 2018-2025, Texas Instruments Incorporated