Vision Apps Release Notes

Version: 11.02.00

Contents

  1. Introduction
  2. Licensing
  3. Getting Started
  4. Documentation
  5. What's New
  6. Device Support
  7. Validation Information
  8. Fixed Issues
  9. Open Defects
  10. Technical Support
  11. Package Versioning


Introduction

The Vision Apps package consists of ADAS, vision, deep learning, perception demos/applications for J722S platform

To run the demos in vision apps, the companion PROCESSOR-SDK-LINUX-J722S also needs to be downloaded separately.


Licensing

Refer to Processor SDK RTOS manifest at top level [HTML]


Getting Started

The Vision Apps User Guide [HTML] provides the documentation and references necessary to begin development on TI's platforms using Vision Apps.


Documentation

Refer to following documentation for further details:

Vision Apps User Guide Build instructions, API Guide [HTML]
Release Notes Archive Previous release notes [FOLDER]


What's New

New features in this release are highlighted in bold


Device Support

Refer Processor SDK RTOS release notes [HTML]

Validation Information

The tools used to validate this package are listed in top level user guide [HTML]


Fixed Issues

ID Summary
ADASVISION-6634 make sbl_bootimage fails from top level SDK build
ADASVISION-6810 J722S memory map conflicts between sysconfig and gen_linker
ADASVISION-6871 UDMA/DRU isn't enabled for the C7x2 on the J722S
ADASVISION-6824 SDK documentation having wrong TI ARM R5F CGT (compiler) version
ADASVISION-6724 Object detection demo block diagram needs to be updated in user guide
ADASVISION-6816 edgeai_deps build failure when TARGET_CPU is not A-core or X86
ADASVISION-6309 Yocto build target is failing with BUILD_CSITX flag set to NO
ADASVISION-6947 [EDGEAI] yaml-cpp/yaml.h: No such file or directory
ADASVISION-6680 J722S: SAFERTOS integration with repo_manifests, app_utils, sdk_builder & vision_apps
ADASVISION-7196 J722S: MCU2_0 DEBUG BINARY FIRMWARE CRASHING on 11.02.00.10 tag


Open Defects

ID Summary
ADASVISION-6451 mailbox queue overflowing while running vx_app_arm_ipc.out
ADASVISION-6473 Multi-cam codec app fails on QNX
ADASVISION-6520 [J722S/J7AEN] DOF: Display2 with PipeID 1 fails to create
ADASVISION-6564 Vision app utils: qnx: All thread creation must use default stack instead of global stack
ADASVISION-6621 Memory map tool does not update sysconfig files if addresses change
ADASVISION-7165 Single and Multi cam have intermittent back to back failure with Fusion2
ADASVISION-6992 [J722S/J7AEN]: SRV demo docs and run scripts missing
ADASVISION-6564 Vision app utils: qnx: All thread creation must use default stack instead of global stack
ADASVISION-6705 [QNX] Check the usage of archiver and fix with standard qcc way


Technical Support

For technical support and additional assistance, contact local TI Field Application Engineer


Package Versioning

Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.

Digit Meaning Description
1 (M=Major) Major revision Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered.
2 (m=minor) Minor revision Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set.
3 (p=patch) Patch number Incremented for all other source code changes. This include any packaging support code.
4 (b=build) Build number Incremented for each release delivery to CM. Reset for any change to M, m or p

Copyright 2020, Texas Instruments Incorporated