![]() |
TISP User Guide
|
Go to the source code of this file.
Macros | |
| #define | MISC_BLOCK_COPY_CYCLES ((NUM_POINTS * NUM_CHANNELS) / 4) |
| #define | FFTLIB_FFT1DBATCHED_32X512_CYCLES (25592) |
| #define | DSPLIB_SQR_CYCLES ((NUM_POINTS * NUM_CHANNELS) / 4) |
| #define | ESITMATED_TOTAL_CYCLE_COUNT ((MISC_BLOCK_COPY_CYCLES + FFTLIB_FFT1DBATCHED_32X512_CYCLES) + DSPLIB_SQR_CYCLES) |
Functions | |
| void | TISP_1dBatched_test_cn (float *pX, float *pW, float *pY0, float *pY1, size_t numPoints, size_t numChannels) |
| void * | create_graph () |
| void | execute_graph (void *myGraph) |
| void | check_output () |
| void | delete_graph (void *myGraph) |
| #define MISC_BLOCK_COPY_CYCLES ((NUM_POINTS * NUM_CHANNELS) / 4) |
Definition at line 11 of file TISP_fft1dBatched_test.cpp.
| #define FFTLIB_FFT1DBATCHED_32X512_CYCLES (25592) |
Definition at line 12 of file TISP_fft1dBatched_test.cpp.
| #define DSPLIB_SQR_CYCLES ((NUM_POINTS * NUM_CHANNELS) / 4) |
Definition at line 13 of file TISP_fft1dBatched_test.cpp.
| #define ESITMATED_TOTAL_CYCLE_COUNT ((MISC_BLOCK_COPY_CYCLES + FFTLIB_FFT1DBATCHED_32X512_CYCLES) + DSPLIB_SQR_CYCLES) |
Definition at line 14 of file TISP_fft1dBatched_test.cpp.
| void TISP_1dBatched_test_cn | ( | float * | pX, |
| float * | pW, | ||
| float * | pY0, | ||
| float * | pY1, | ||
| size_t | numPoints, | ||
| size_t | numChannels | ||
| ) |
Definition at line 202 of file TISP_1dBatched_test_cn.cpp.
| void* create_graph | ( | ) |
[connecting nodes example]
[connecting nodes example]
Definition at line 21 of file TISP_fft1dBatched_test.cpp.
| void execute_graph | ( | void * | myGraph | ) |
Definition at line 64 of file TISP_fft1dBatched_test.cpp.
| void check_output | ( | ) |
Definition at line 87 of file TISP_fft1dBatched_test.cpp.
| void delete_graph | ( | void * | myGraph | ) |
Definition at line 110 of file TISP_fft1dBatched_test.cpp.