9.9. Adding new image sensor to PSDK RTOS

9.9.1. Introduction

Imaging library is a collection of sample algorithms and image sensor drivers packaged with PSDK RTOS to enable camera based applications. It includes sensor driver framework which is a modular and extensible framework to

  • Add new sensor drivers easily.

  • Provide a consistent interface to applications and algorithms.

The goal of this framework is to add new sensors with zero code modifications to the applications. Any application using an image sensor is expected to be agnostic to the underlying HW. The application is expected to communicate with the driver framework using RPC commands. The details of supported sensors and the sensor capabilities are queried at runtime.

Similarly algorithms communicating with image sensor (e.g. AutoExposure) are required to send RPC commands at runtime without knowing which sensor is operational. Driver framework is responsible for mapping the camera ID to the associated physical image sensor.

This mechanism allows algorithm and application code to remain unchanged as new sensors are added to the framework.

9.9.2. Documentation References

SDK Component

Documentation

Description

Section

vision apps

LINK

Single Camera VPAC Demo

Application / Demos > Basic Demos > Single Camera VPAC Application

vision apps

LINK

Multi Camera VPAC Demo

Application / Demos > Basic Demos > Multi Camera VPAC Application

imaging

LINK

Imaging drivers and algos

Imaging / Modules > Imaging Sensor Driver Modules

9.9.3. Source Code References

SDK Component

File / Folder

Description

Imaging

imaging/sensor_drv

Sensor driver source code

vision apps

vision_apps/utils/iss

Common ISS Utilities to be used by all camera based applications

vision apps

vision_apps/apps/basic_demos/app_single_cam

Demo Application using a single camera instance

vision apps

vision_apps/apps/basic_demos/app_multi_cam

Demo Application using a multiple (upto 8) camera instances

9.9.4. Key Data Structures

9.9.4.1. IssSensor_CreateParams

Create time parameters like width, height, dataformat, I2C address for the image sensor. For more details, please refer to imaging/sensor_drv/include/iss_sensor.h

9.9.4.2. IssSensorFxns

Set of callbacks of all routines to be implemented by the sensor driver. For more details, please refer to imaging/sensor_drv/include/iss_sensor.h

9.9.4.3. IssSensorIntfParams

Interface parameters e.g. number of CSI-2 date lanes, position, polarity etc. For more details, please refer to imaging/sensor_drv/include/iss_sensor.h

9.9.4.4. I2cParams

Struct containing register address, value and delay (milli seconds). For more details, please refer to imaging/sensor_drv/include/iss_sensor.h

9.9.4.5. IssSensorConfig

Struct containing pointers to sensor and SerDes configuration structures.

Note

  • Last entry in Serializer and Deserializer config scripts must be {0xFFFF, 0x00, 0x0}

9.9.4.6. IssSensors_Handle

Handle to the image sensor driver including all the information about the sensor For more details, please refer to imaging/sensor_drv/include/iss_sensor.h

9.9.5. Application - Driver Interface

9.9.5.1. RPC Commands

Application communicates with the sensor driver using RPC (Remote Procedure Call) commands The commands defined currently are listed below.

Command

Description

IM_SENSOR_CMD_ENUMERATE

Called by the application to get a list of names of all the sensors supported.

IM_SENSOR_CMD_QUERY

Called by the application to query the capabilities of an image sensor by name.

IM_SENSOR_CMD_PWRON

Called by the application to power ON the sensor. Sensor f/w invokes powerOn callback of the selected sensor. Exact implementation of this function is left to the specific sensor driver.

IM_SENSOR_CMD_PWROFF

Called by the application to power OFF the sensor. Sensor f/w invokes powerOff callback of the selected sensor. Exact implementation of this function is left to the specific sensor driver.

IM_SENSOR_CMD_STREAM_ON

Called by the application to start streaming. Sensor f/w invokes streamOn callback of the selected sensor. Exact implementation of this function is left to the specific sensor driver.

IM_SENSOR_CMD_STREAM_OFF

Called by the application to stop streaming. Sensor f/w invokes streamOff callback of the selected sensor. Exact implementation of this function is left to the specific sensor driver.

IM_SENSOR_CMD_CTL

Called by the application to send runtime control commands. Next section describes the runtime controls currently supported.

IM_SENSOR_CMD_DEBUG

Called by the application for advanced debugging support.

9.9.5.2. Control Commands

IM_SENSOR_CMD_STREAM_CTL command can have an argument for control command. Control commands defined currently are listed below.

Command

Description

IMAGE_SENSOR_CTRLCMD_GETEXPPRG

Typically called by the AutoExposure algorithm to know sensor’s exposure constraints, which can then be used for initializing AutoExposure algorithm.

IMAGE_SENSOR_CTRLCMD_GETWBCFG

Typically called by the AutoWhiteBalnce algorithm to know sensor’s WB constraints, which can then be used for initializing AutoWhiteBalance algorithm. This is needed only if WB gains are to be applied in sensor vs ISP.

IMAGE_SENSOR_CTRLCMD_SETEXPGAIN

Typically called by the AutoExposure algorithm to set exposure time and analog/digital gain. Sensor f/w invokes setAeParams callback of the selected sensor. Exact implementation of this function is left to the specific sensor driver.

IMAGE_SENSOR_CTRLCMD_GETEXPGAIN

Reserved for future use.

IMAGE_SENSOR_CTRLCMD_SETWBGAIN

Typically called by the AutoWhiteBalance algorithm to set color gains. Sensor f/w invokes setAwbParams callback of the selected sensor. Exact implementation of this function is left to the specific sensor driver.

IMAGE_SENSOR_CTRLCMD_GETWBGAIN

Reserved for future use.

IMAGE_SENSOR_CTRLCMD_READ_SENSOR_REG

Used for reading or writing sensor/serilaizer/deserializer registers through a script.

IMAGE_SENSOR_CTRLCMD_WRITE_SENSOR_REG

Used for reading or writing sensor/serilaizer/deserializer registers through a script.

Note

Command set may be extended in future

9.9.6. Steps to create a new sensor driver

9.9.6.1. Create a folder

Create a new folder inside imaging/sensor_drv/src/ e.g. <newsensor123>

9.9.6.2. Create sensor driver file

Create a new source file implementing all the structures and callbacks mentioned in Key Data Structures.

9.9.6.2.1. createParams

Parameter

Usage

name

Pick any unique string no longer than 32 characters

i2cInstId

Specify I2C channel on which the sensor is connected. For Jacinto 7 EVM, default is 0x6

i2cAddrSensor

Array of sensor address aliases. Upto 8 instances supported. Must match alias values specified in UB960 config.

Note

If the sensor is connected directly i.e. without SerDes, provide sensor’s physical I2C address (7-bit) here

i2cAddrSer

Array of serializer address aliases. Upto 8 instances supported. Must match alias values specified in UB960 config.

width

Number of pixels per line in sensor output, not including H blanking.

height

Number of lines per frame in sensor output, not including V blanking or metadata.

num_exposures

Number of exposure channels per frame.

line_interleaved

Reserved for future use.

pixel_container

width of container element.

msb

MSB of valid data. Must be set to bpp -1. E.g. MSB = 11 for 12b RAW.

features

Binary mask specifying sensor capabilities.

fps

Frame rate per second. Not used currently.

numDataLanes

Number of CSI-2 data lanes. Must match sensor & deserializer settings.

dataLanesMap

Mapping of sensor CSI2 lanes to CSI2 Rx. Must match sensor & deserializer settings.

dataLanesPolarity

Reserved for future use.

csi_ddr_clock

Reserved for future use.

num_channels

Number of camera instances supported. Valid values : 1-8.

dccId

Unique numerical identfier. Used for ISP tuning.

9.9.6.2.2. IssSensorFxns

API Name

Description

probe

Detects if sensor is accessible, usually by reading sensor chip ID.

config

Configures serializer and sensor. Argument sensor_features_requested maybe used to load different configuration based on application request. For e.g 30fps mode vs 60fps mode.

streamOn

Enables streaming on sensor and deserializer.

streamOff

Disables streaming on sensor and deserializer.

powerOn

HW dependent. Pull up/down any GPIOs, if needed. Configures the deserializer so that sensor is accessible over FPD Link backchannel.

powerOff

HW dependent. Pull up/down any GPIOs, if needed.

getExpParams

Reserved for future use. Must be implemented as a dummy function returning 0.

setAeParams

Translates AE computed exposure time and analog gain to sensor specific settings. Updates sensor registers with new values.

getDccParams

Reserved for future use. Must be implemented as a dummy function returning 0.

initAewbConfig

Reserved for future use. Must be implemented as a dummy function returning void.

getIspConfig

Reserved for future use. Must be implemented as a dummy function returning void.

readWriteReg

Reserved for future use. Must be implemented as a dummy function returning 0.

getExpPrg

Called by AE algorithm to get the sensor exposure constraints.

deinit

Reserved for future use. Must be implemented as a dummy function returning void.

Note

For more details, please refer to an existing sensor driver

9.9.6.3. Update makefile

Modify sensor_drv/src/concerto.mak to add the newly added sensor file. For e.g.

CSOURCES += newsensor123/iss_sensor_newsensor123.c

9.9.6.4. Register the new sensor with framework

Modify the function IssSensor_Init in the file sensor_drv/src/iss_sensors.c to call init function of the new sensor. For e.g.

status |= IssSensor_NewSensor123_Init();

9.9.6.5. Build and Run

  • Do a clean build of imaging, followed by sdk build.

  • Upon execution, new sensor should be populated in the enumerated sensor list.

  • Select the sensor and run. If the sensor and SerDes settings are correct, a preview should be displayed on the connected display.

  • At this stage, sensor driver is functional. However, image quality may not be perfect.

  • Please refer to DCC Tuning Tool documentation for the steps to achieve good image quality using TI ISP.