9.11. Running SDE and DOF for 2M-Pixel Input

9.11.1. Introduction

The Stereo Depth Engine (SDE) and Dense Optical Flow (DOF) HWAs are designed to process the input resolution up to 2048x1024. However, due to the limited size of a SL2 memory block that serves both SDE and DOF, they cannot process 2M-pixel inputs at the same time. By default, SDE and DOF are assigned SL2 memory for the input sequences with smaller horizontal size and smaller search range than supported. For example, the default SL2 memory mapping allows SDE to process up to 1280 horizontal pixels with disparity search range of 128 and allows DOF to process up to 1312 horizontal pixels with vertical search range of -48 ~ +48. Note that the maximum disparity search range for SDE is 192 and the maximum vertical search range for DOF is -62 ~ +62.

Therefore, in order for either SDE or DOF to process 2M-pixel input with larger search range, SL2 memory should be reallocated. This developer note explains how to do it.

9.11.2. DMPAC SL2 Memory Reallocation

To support SL2 memory reallocation for DMPAC, the VHWA remote service handler named APP_VHWA_SERVICE_NAME is registered during the vision_apps initialization step. The VHWA remote service handler receives the four commands as shown in the table below. Note that these commands and related parameters are defined in <SDK_PATH>/vision_apps/utils/hwa/include/app_hwa.h.

Command

Description

APP_DMPAC_SDE_SL2_FREE

Free SL2 memory assigned already for SDE

APP_DMPAC_DOF_SL2_FREE

Free SL2 memory assigned already for DOF

APP_DMPAC_SDE_SL2_REALLOC

Allocate SL2 memory for SDE according to the given SL2 memory parameters

APP_DMPAC_DOF_SL2_REALLOC

Allocate SL2 memory for DOF according to the given SL2 memory parameters

Before reallocating SL2 memory for SDE and DOF, existing SL2 memory should be freed up. The application should call the remote services with APP_DMPAC_SDE_SL2_FREE and APP_DMPAC_DOF_SL2_FREE commands as follows:

int32_t vhwaDmpacSl2Free()
{
    int32_t status;

    status = appRemoteServiceRun(APP_IPC_CPU_MCU2_1, APP_VHWA_SERVICE_NAME,
                                 APP_DMPAC_SDE_SL2_FREE,
                                 NULL, 0, 0);

    if (status == 0)
    {
        status = appRemoteServiceRun(APP_IPC_CPU_MCU2_1, APP_VHWA_SERVICE_NAME,
                                     APP_DMPAC_DOF_SL2_FREE,
                                     NULL, 0, 0);
    }

    return status;
}

Then SL2 memory should be allocated again with desired parameters. For SDE to process 2M-pixel input with 192 disparity search range, the remote service with APP_DMPAC_SDE_SL2_REALLOC command should be called as follows:

int32_t vhwaDmpacSdeSl2Realloc()
{
    int32_t status = 0;

    App_M2mSdeSl2AllocPrms sl2AllocPrms;

    // Reset parameters
    sl2AllocPrms.maxImgWidth  = 2048;
    sl2AllocPrms.inCcsf       = APP_FVID2_CCSF_BITS12_UNPACKED16;
    sl2AllocPrms.searchRange  = APP_SDE_SR_192;
    sl2AllocPrms.disBuffDepth = APP_SDE_DEFAULT_DIS_BUFF_DEPTH;

    status = appRemoteServiceRun(APP_IPC_CPU_MCU2_1, APP_VHWA_SERVICE_NAME,
                                 APP_DMPAC_SDE_SL2_REALLOC,
                                 &sl2AllocPrms, sizeof(sl2AllocPrms), 0);

    return status;
}

Similarly, for DOF to process 2M-pixel input with vertical search range of -62 ~ +62, the remote service with APP_DMPAC_DOF_SL2_REALLOC command should be called as follows:

int32_t vhwaDmpacDofSl2Realloc()
{
    int32_t status = 0;

    App_M2mDofSl2AllocPrms sl2AllocPrms;

    // Reset parameters
    sl2AllocPrms.maxImgWidth   = 2048;
    sl2AllocPrms.inCcsf        = APP_FVID2_CCSF_BITS12_UNPACKED16;
    sl2AllocPrms.refBuffDepth  = APP_DOF_DEFAULT_REF_BUFF_DEPTH;
    sl2AllocPrms.currBuffDepth = APP_DOF_DEFAULT_CUR_BUFF_DEPTH;
    sl2AllocPrms.fvBuffDepth   = APP_DOF_DEFAULT_FV_BUFF_DEPTH;
    sl2AllocPrms.topSR         = 62;
    sl2AllocPrms.botSR         = 62;

    status = appRemoteServiceRun(APP_IPC_CPU_MCU2_1, APP_VHWA_SERVICE_NAME,
                                 APP_DMPAC_DOF_SL2_REALLOC,
                                 &sl2AllocPrms, sizeof(sl2AllocPrms), 0);

    return status;
}

9.11.3. SDE and DOF Demos for 2M-Pixel Input

Let us take examples of <SDK_PATH>/vision_apps/apps/basic_demos/app_stereo and <SDK_PATH>/vision_apps/apps/basic_demos/app_dof to see what should be added for SDE and DOF demos to support 2M-pixel input with larger search range.

9.11.3.1. SDE Demo

app_init() function in <SDK_PATH>/vision_apps/apps/basic_demos/app_stereo/main.c should be modified as shown below. Note that vhwaDmpacSl2Free() and vhwaDmpacSdeSl2Realloc(), which are introduced in the previous section, are called.

static vx_status app_init(AppObj *obj)
{

    vx_status status = VX_SUCCESS;
    app_grpx_init_prms_t grpx_prms;


#if !defined(PC)
    // Free SDE and DOF SL2
    vhwaDmpacSl2Free();

    // Reallocate SDE SL2
    vhwaDmpacSdeSl2Realloc();
#endif

    obj->context = vxCreateContext();
    status = vxGetStatus((vx_reference)obj->context);
    if(status == VX_SUCCESS)
    {
        tivxStereoLoadKernels(obj->context);
        tivxHwaLoadKernels(obj->context);
    }
    ...

}

9.11.3.2. DOF Demos

app_init() function in <SDK_PATH>/vision_apps/apps/basic_demos/app_dof/main.c should be modified as shown below. Note that vhwaDmpacSl2Free() and vhwaDmpacDofSl2Realloc(), which are introduced in the previous section, are called.

static vx_status app_init(AppObj *obj)
{
    app_grpx_init_prms_t grpx_prms;
    vx_status status = VX_SUCCESS;


#if !defined(PC)
    // Free SDE and DOF SL2
    vhwaDmpacSl2Free();

    // Reallocate SDE SL2
    vhwaDmpacDofSl2Realloc();
#endif


    obj->context = vxCreateContext();
    if(status == VX_SUCCESS)
    {
        status = vxGetStatus((vx_reference) obj->context);
    }

    tivxHwaLoadKernels(obj->context);
    ...

}