EthFw Release Notes
Version: 11.02.00
Contents
- Introduction
- Licensing
- Getting Started
- Documentation
- Device Support
- Validation Information
- Limitations
- Dependencies
- Technical Support
- Package Versioning
Introduction
This release notes provides important information that will assist you in using the EthFw component. This document provides the product information and known issues with respect to EthFw software component. The EthFw component consists of firmware for Ethernet switch, profiling tools and demos/applications for J722S silicon platforms.
Licensing
Refer to Processor SDK RTOS top-level manifest.
Getting Started
The Ethernet Firmware User's Guide provides the documentation and references necessary to run EthFw demos and begin development on TI's platforms.
Documentation
Refer to following documentation for further details:
| Ethernet Firmware User Guide | Build instructions, Demos | User Guide |
| Ethernet Firmware API Guide | API Guide | API Guide |
Device Support
Below table shows device support for EthFw.| SoC | HOST (OS) | Target (OS) | Test Platform |
| J722S | Linux | FreeRTOS | J722S EVM |
Refer Processor SDK RTOS release notes for SDK device support.
Validation Information
This release was built and validated using the following tools. Refer to the EthFw User's Guide for additional instructions to install and setup the dependencies.Build Tools (included in Processor SDK)
- TI ARM CLANG: 4.0.4.LTS
- lwIP stack: 2.2.1
- FreeRTOS Kernel: 11.1.0
Limitations
MAC Port 2 supports SGMII mode via MAC-to-MAC connectivity to another Jacinto device (e.g., J721E) through an Ethernet Expander Bridge, as J722S lacks integrated SGMII PHY support.
Dependencies
All Ethernet Firmware dependencies are also part of the SDK, please refer to the User's Guide for details.
Technical Support
For technical support and additional assistance, contact local TI Field Application Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.
| Digit | Meaning | Description |
|---|---|---|
| 1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
| 2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
| 3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
| 4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p. |
Copyright 2023, Texas Instruments Incorporated