VHWA Introduction
Contents
- Introduction
- Licensing
- Documentation
- What's New
- Fixed Issues
- Known Issues
- VHWA Test Application
- Technical Support
- Package Versioning
- Trainings
Introduction
The Vision Hardware Accelerator (VHWA) provides the logic to interface for MSC, NF, LDC, VISS, DOF and SDE accelerators. This is VHWA FVID2 driver documentation.
Licensing
Documentation
| VHWA Static Analysis Report | Static Analysis Report | [XLSX] |
| VHWA Driver API Guide | API Guide | [HTML] |
| VHWA Standalone applications performance | Performance Statistics | [XLSX] |
| VHWA Test Report (AM62A) | Test Report | [XLSX] |
| VHWA Bidirectional Report (AM62A) | Bi-Directional Traceability Report | [XLSX] |
| VHWA Test Report (J7AEN) | Test Report | [XLSX] |
| VHWA Bidirectional Report (J7AEN) | Bi-Directional Traceability Report | [XLSX] |
What's New
- Disabling of Error Interrupts support in VHWA for all platforms. A feature has been enabled for all VHWA modules which allows the users to enable/disable error interrupts, including the watchdog timer error interrupt.
- VHWA (VPAC and DMPAC) low-level drivers (VISS, MSC, LDC, DOF, SDE) on J7-AEN device is ready for ASIL-B safety certification. CSP package will be made available upon request.
- VHWA (VPAC) low-level drivers (VISS, MSC, LDC,) on AM62a device is ready for ASIL-B safety certification. CSP package will be made available upon request.
- RTOS VPAC3L driver on Main R5 - DMA-based register configuration support for VISS now available for J7-AEN platform.
Fixed Issues
| ID | Summary |
|---|---|
| PDK-19301 | MISRA and static analysis fixes for VPAC and DMPAC driver |
| PDK-18759 | tivxEventPost is called multiple times for the same frame due to error interrupt callbacks |
| PDK-19117 | Incorrect Error Interrupt Masks for VISS based on IP revisions |
| PDK-18772 | An IP in a stalled state allows process requests submission, resulting in a stall |
| PDK-19010 | VHWA: Kernel tap params configured for non-applicable modules. |
| PDK-19129 | VPAC LDC: Bandwidth limiter settings applied to one handle unintentionally affect all other handles |
| PDK-19141 | VHWA:MSC: Single-phase coefficients not cleared when switching to multiphase coefficients between test cases |
| PDK-19142 | VHWA:HTS: Duplicate configuration of pattern adaptor enable bit leading to readback mismatch |
| PDK-19029 | VHWA-SDE confidence score map incorrectly programmed for map value > 7 |
| PDK-19143 | VHWA:MSC: Incorrect Configuration Readback in MSC Sequential Processing |
| PDK-17427 | [VHWA]: Added mechanism to modify WDG Timeout cycles for all modules |
| PDK-19173 | Fixed issue where enabling/disabling Error Interrupts for VISS, SDE, and NF did not take effect if the control command was invoked between frame processing for the same handle. |
| PDK-19177 | Resolved improper masking issue causing errors when enabling Watchdog Timer Error Interrupt or Event Interrupts for VISS. |
Known Issues
| ID | Summary |
|---|---|
| PDK-12683 | Chroma only output is not correct from Human Vision Pipeline when machine vision is enabled. |
| PDK-12681 | Incorrect access of luma and chroma channel in luma only and chroma only mode causes corruption. |
| PDK-13247 | AEWB output incorrect for VISS for Three Frame Merge with two YUV420, saturation and AEWB output |
| PDK-12860 | [VHWA-VISS]: Error check missing while setting VISS module specific configuration |
| - | [VHWA]: DPC stats enable MMR is not configurable from VHWA VPAC3L. |
| - | [VHWA]: DCC live tuning for AWB is not working properly on AM62A |
| - | [VHWA]: GLBCE context save and restore requires validation using low level driver test case for J722S and AM62A |
| - | [DMPAC]: DOF and SDE performance numbers are not meeting expectation on J722S |
| - | [VPAC]: AF output incorrect for VISS for Three Frame Merge with two YUV420, saturation and AF output |
| PDK-19176 | Updating Configurations for SDE will not take effect if the control command for the same is invoked between frame processing for the same handle. |
| SITSW-11754 / PDK-20284 | Failure on Flexconnect Safety test case related to 3 inputs to VISS |
| SITSW-11753 / PDK-20392 | Failure on CSL_nsf4vSetConfig VISS-PCID test case for AM62A / J722S |
| SITSW-11752 / PDK-20393 | Failure on "VISS-PCID for single RAW input and irRemapLut Enabled 1920x1080 - YUV, IR" test case for AM62A / J722S |
| SITSW-11992 / PDK-20394 | H3a output mismatch for LLD testcases on AM62A / J722S |
Application Examples
| VHWA Module | Test Application | Supported Platform | Supported Cores |
|---|---|---|---|
| VISS | baremetal, freertos, safertos baremetal, freertos, safertos baremetal, freertos, safertos baremetal, freertos baremetal, freertosbaremetal, freertos |
J721S2 J721E J784S4 J742S2 J722SAM62A |
mcu2_0 mcu2_0 mcu2_0, mcu4_0 mcu2_0, mcu4_0 main_r5wakeup_r5 |
| LDC | baremetal, freertos, safertos baremetal, freertos, safertos baremetal, freertos, safertos baremetal, freertos baremetal, freertosbaremetal, freertos |
J721S2 J721E J784S4 J742S2 J722SAM62A |
mcu2_0 mcu2_0 mcu2_0, mcu4_0 mcu2_0, mcu4_0 main_r5wakeup_r5 |
| MSC | baremetal, freertos, safertos baremetal, freertos, safertos baremetal, freertos, safertos baremetal, freertos baremetal, freertosbaremetal, freertos |
J721S2 J721E J784S4 J742S2 J722SAM62A |
mcu2_0 mcu2_0 mcu2_0, mcu4_0 mcu2_0, mcu4_0 main_r5wakeup_r5 |
| DOF | baremetal, freertos, freertos-negative, safertos baremetal, freertos, safertos baremetal, freertos, freertos-negative, safertos baremetal, freertos, freertos-negative baremetal, freertosbaremetal, freertos |
J721S2 J721E J784S4 J742S2 J722SAM62A |
mcu2_1 mcu2_1 mcu2_1 mcu2_1 main_r5wakeup_r5 |
| SDE | baremetal, freertos, freertos-negative, safertos baremetal, freertos, safertos baremetal, freertos, freertos-negative, safertos baremetal, freertos, freertos-negative baremetal, freertosbaremetal, freertos |
J721S2 J721E J784S4 J742S2 J722SAM62A |
mcu2_1 mcu2_1 mcu2_1 mcu2_1 main_r5wakeup_r5 |
Steps to run VHWA test applications:
For VPAC1 and VPAC3 devices
cd pdk/packages/ti/drv/vhwa/
make help
VHWA example build
make vhwa_msc_baremetal_testapp BOARD=j721s2_evm SOC=j721s2 CORE=mcu2_0 BUILD_PROFILE=debug
For VPAC3L devices:
Navigate to mcu_plus_sdk path
make DEVICE=j722s gen-buildfiles
cd test/unity/
make -f makefile.j722s.r5f.ti-arm-clang
cd ../../
make -s -f makefile.j722s all DEVICE=j722s PROFILE=release
make -C source/drivers/vhwa -f makefile.j722s.main-r5fss0-0.ti-arm-clang PROFILE=release
Steps to run DOF, SDE Negative test applications:
For VPAC3 devices
cd pdk/packages/ti/drv/vhwa/
make help
Build the negative test application using the following command:
make vhwa_sde_negative_testapp_freertos BOARD=j721s2_evm SOC=$SOC CORE=mcu2_1 BUILD_PROFILE=release VHWA_NEGATIVE_TEST=true
For negative test with FOCO WDTimer error, change the true flag like so:
make vhwa_sde_negative_testapp_freertos BOARD=j721s2_evm SOC=$SOC CORE=mcu2_1 BUILD_PROFILE=release VHWA_NEGATIVE_FOCO_TEST=true
The test binary will be created at the following path:
pdk/packages/ti/binary/vhwa_sde_testapp_freertos/bin/j721s2_evm/vhwa_sde_testapp_freertos_mcu2_1_debug.xer5f
Load this binary and run the application.
To trigger the watchdog timer error, run testcase 3. This is applicable for DOF, SDE and (DOF, SDE) IP's FOCO watchdog timer error.
NOTE: Test case 3 Image Resolution:
DOF: 2 MP, 8-bit
SDE: 1 MP, 8-bit
Technical Support
For technical support and additional assistance, contact E2E Forum
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.
| Digit | Meaning | Description |
|---|---|---|
| 1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
| 2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
| 3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
| 4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
Trainings
| VHWA Overview | VHWA Modules and SW Overview | [PPTX] |
[PDF] |
Copyright 2024, Texas Instruments Incorporated