70 #ifndef NETWORK_API_H_ 71 #define NETWORK_API_H_ 82 #include <sys/types.h> 83 #include <sys/socket.h> 85 #include <netinet/in.h> 87 #include <sys/select.h> 89 #include <sys/types.h> 94 #include <sys/ioctl.h> Definition: network_api.h:110
int32_t Network_waitConnect(Network_SockObj *pObj, uint32_t timeout)
int sockFd
Definition: network_api.h:112
unsigned int port
Definition: network_api.h:115
int32_t Network_close(Network_SockObj *pObj, Bool closeServerSock)
int32_t Network_open(Network_SockObj *pObj, uint32_t port)
int Bool
Definition: network_api.h:105
int connectedSockFd
Definition: network_api.h:118
int32_t Network_read(Network_SockObj *pObj, uint8_t *dataBuf, uint32_t *dataSize)
int32_t Network_write(Network_SockObj *pObj, uint8_t *dataBuf, uint32_t dataSize)