34 #ifndef MATHLIB_ATAN2_H_
35 #define MATHLIB_ATAN2_H_
43 #include "../common/MATHLIB_types.h"
121 MATHLIB_atan2_dp(
size_t length,
double* pSrc0,
double* pSrc1,
double* pDst);
MATHLIB_STATUS MATHLIB_atan2_dp(size_t length, double *pSrc0, double *pSrc1, double *pDst)
This function is the C interface for MATHLIB_atan2. Function accepts double pointers.
MATHLIB_STATUS MATHLIB_atan2(size_t length, T *pSrc0, T *pSrc1, T *pDst)
Performs the elementwise arc-tangent2 of the input vector. Function can be overloaded with float and ...
MATHLIB_STATUS MATHLIB_atan2_sp(size_t length, float *pSrc0, float *pSrc1, float *pDst)
This function is the C interface for MATHLIB_atan2. Function accepts float pointers.
MATHLIB_STATUS_NAME
The enumeration of all status codes.