Vision Apps Release Notes

Version: 10.00.00

Contents

  1. Introduction
  2. Licensing
  3. Getting Started
  4. Documentation
  5. What's New
  6. Device Support
  7. Validation Information
  8. Fixed Issues
  9. Open Defects
  10. Known Issues
  11. Change Requests
  12. Technical Support
  13. Package Versioning


Introduction

The Vision Apps package consists of ADAS, vision, deep learning, perception demos/applications for J722S platform

To run the demos in vision apps, the companion PROCESSOR-SDK-LINUX-J722S also needs to be downloaded separately.


Licensing

Refer to Processor SDK RTOS manifest at top level [HTML]


Getting Started

The Vision Apps User Guide [HTML] provides the documentation and references necessary to begin development on TI's platforms using Vision Apps.


Documentation

Refer to following documentation for further details:

Vision Apps User Guide Build instructions, API Guide [HTML]
Release Notes Archive Previous release notes [FOLDER]


What's New

New features in this release are highlighted in bold


Device Support

Refer Processor SDK RTOS release notes [HTML]

Validation Information

The tools used to validate this package are listed in top level user guide [HTML]


Fixed Issues

ID Summary
ADASVISION-6279 SDK documentation require update for vision_apps memory map
ADASVISION-6265 app_multi_cam crashes during tear down
ADASVISION-6254 App c7x hang
ADASVISION-6243 app_ stereo does not show graphics properly
ADASVISION-6242 app_dof does not work properly
ADASVISION-6179 QNX: FD exchange app fails
ADASVISION-6295 Failure in CSITx for UDMA channel configuration when enabling from Vision-Apps


Open Defects

ID Summary
ADASVISION-6315 DOF: Display2 with PipeID 1 fails to create
ADASVISION-6311 4 Camera IMX219 GStreamer Pipeline Failure
ADASVISION-6286 Memory map alignment of VRING sections is invalid
ADASVISION-6266 tivxWriteImageNode incorrect save for YUV422 format
ADASVISION-6212 MACRO RGB888_TO_RGB565 should be RGB888_TO_BGR565 in the Draw2D utility


Known Issues

ID Summary Workaround
ADASVISION-4345 SteamFIFO overflow observed in long run > 6hrs when using D3 IMX390 CM cameras Upgrade to D3 IMX390 RCM cameras

Change Requests

ID Headline Original Fix Version New Fix Version
NA NA NA NA


Technical Support

For technical support and additional assistance, contact local TI Field Application Engineer


Package Versioning

Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.

Digit Meaning Description
1 (M=Major) Major revision Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered.
2 (m=minor) Minor revision Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set.
3 (p=patch) Patch number Incremented for all other source code changes. This include any packaging support code.
4 (b=build) Build number Incremented for each release delivery to CM. Reset for any change to M, m or p

Copyright 2020, Texas Instruments Incorporated