Vision Apps Datasheet
Vision Apps Datasheet
  1. Basic Demos Datasheets
  2. DL Demos Datasheets

Legend

Each of the datasheets in this document are automatically generated at run-time using performance and memory statistics collection libraries running across the SoC.

Each core may have different memories that it considers L3_MEM heap. The following table can be used to identify which physical memory is being referred to by L3_MEM heap for each core.

Core L3_MEM Location --—
MCU2_0 OCRAM (256 KB)
c7x_1 L2 (2.25MB)
c7x_2 L2 (2.25MB)

Additionally, each core is using a default frequency which is used out of box and was the frequency used when generating the performance datasheets.

Core Frequency --------—
R5F Cores 800 Mhz
C7X Cores 1 GHz
VPAC 600 MHz
DMPAC 420 MHz