J722S MCU+ SDK  10.00.00
SBL SD HLOS

Introduction

This is a bootloader example, which shows an example of booting Linux/U-Boot/QNX on A53 core and RTOS/NORTOS applications on DM R5 and M4 cores. This SBL target supports booting the following test cases

  • SBL Booting Linux Kernel
  • SBL Booting U-Boot
  • SBL Booting QNX

Supported Combinations

Parameter Value
CPU + OS wkup-r5fss0-0 nortos
Toolchain ti-arm-clang
Board j722s-evm
Example folder examples/drivers/boot/sbl_ospi_hlos

Steps to Run the Example

Prepare the SD Card

  • Create SD card using balena etcher tool, refer Processor-SDK-Linux for more details
  • This is needed to have file system in root partition of SD card

Build the Example

  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Create Linux Appimage

  • Create a Linux Appimage containing the Linux binaries (ATF, OPTEE, A53 SPL) or (ATF, OPTEE, Kernel, DTB) in case of fastboot mode.
  • This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/linuxAppimageGen after setting the PSDK path in file config.mak
  • Refer Linux Appimage Generator Tool for more details

Create QNX Appimage

  • Create a QNX Appimage containing (TAF, OPTEE, QNX-IFS)
  • This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/qnxAppimageGen after setting the PSDK path in file config.mak
  • Refer QNX Appimage Generator Tool for more details

Run the example

  • Copy SBL image as tiboot3.bin to the boot partition of SD card
  • Copy HLOS appimage as app to the boot partition of SD card
  • Copy u-boot.img to the boot partition of SD card in case booting U-Boot
  • Boot the EVM in SD boot mode.

See Also

BOOTLOADER