Introduction
This is a bootloader example, which shows an example of booting Linux/U-Boot/QNX on A53 core and RTOS/NORTOS applications on DM R5 and M4 cores. This SBL target supports booting the following test cases
- SBL Booting Linux Kernel
- SBL Booting U-Boot
- SBL Booting QNX
Supported Combinations
| Parameter | Value |
| CPU + OS | wkup-r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | j722s-evm |
| Example folder | examples/drivers/boot/sbl_ospi_hlos |
Steps to Run the Example
Prepare the SD Card
- Create SD card using balena etcher tool, refer Processor-SDK-Linux for more details
- This is needed to have file system in root partition of SD card
Build the Example
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Create Linux Appimage
- Create a Linux Appimage containing the Linux binaries (ATF, OPTEE, A53 SPL) or (ATF, OPTEE, Kernel, DTB) in case of fastboot mode.
- This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/linuxAppimageGen after setting the PSDK path in file
config.mak
- Refer Linux Appimage Generator Tool for more details
Create QNX Appimage
- Create a QNX Appimage containing (TAF, OPTEE, QNX-IFS)
- This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/qnxAppimageGen after setting the PSDK path in file
config.mak
- Refer QNX Appimage Generator Tool for more details
Run the Example
See Also
BOOTLOADER