J722S MCU+ SDK  10.00.00
CSIRX CAPTURE TEST

Introduction

In this example, each CSIRX instance in the SOC is configured to receive RAW12 packets from 4 virtual channels

Supported Combinations

Parameter Value
CPU + OS main-r5fss0-0 freertos
Toolchain ti-arm-clang
Board j722s-evm
Example folder examples/drivers/csirx/csirx_capture_test/

Steps to Run the Example

Sample Output