This bootloader does SOC initializations and attempts to boot a multicore appimage present at 0x80000 location in the OSPI Flash. To flash a multicore appimage at this location, follow the steps mentioned in Basic steps to flash files.
If a multicore appimage is found at the location, the SBL parses it, splits it into RPRCs for each core applicable. Each core is then initialized, RPRC image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders
| Parameter | Value |
|---|---|
| CPU + OS | wkup-r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Boards | j722s-evm |
| Example folder | examples/drivers/boot/sbl_ospi |
Since this is a bootloader, the example will be run every time you boot an application using this example. It is run from a OSPI boot media unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.
cd ~/ti/mcu_plus_sdk/tools/boot python uart_uniflash.py -p <main UART COM port> --cfg=~/ti/mcu_plus_sdk/tools/sbl_prebuilt/j722s-evm/default_sbl_ospi_hs_fs.cfg