5.2. VTM Safety Example¶
5.2.1. Introduction¶
This example demonstrates the usage of the VTM to detect overtemperature events and signal the events through the ESM. The example shows how to configure the VTM for the various alerts and listen for VTM events using the ESM. It also shows forcing an error in order to demonstrate application notification of overtemperature events.
The example demonstrates:
Configuring the VTM thresholds
Early alert event detection
Critial threshold event detection
Follow-up event notification when temperature has dropped to a safe level
5.2.2. Use Cases¶
Use Case
Description
ESM
Input Event
UC-1
Configuration of VTM threshold to trigger early warning, then return thresholds back to normal to simulate “cooling down”.
WKUP_ESM0
WKUP_VTM0_THERM_LVL_GT_TH1_INTR_0 Temp greater than early warning threshold
UC-2
Configuration of VTM to trigger early warning, then alter the thresholds again to pass temperature critical threshold. Then, return thresholds back to normal to simulate “cooling down”.
WKUP_ESM0
WKUP_VTM0_THERM_LVL_GT_TH2_INTR_0
5.2.3. Example Details¶
The example should be loaded to the hardware using the Secondary Boot Loader (SBL) from the SDK.
Example Name |
Location |
Build Command |
|---|---|---|
vtm_app |
[sdl_install_dir]/examples/vtm/ |
make vtm_app PROFILE=release |
5.2.4. Expected Output¶
VTM Example Application
VTM_ESM_init: Init WKUP ESM complete
VTM_ESM_init complete
Starting Use Case 0
Got gtThr1 interrupt through ESM module
Crossed early warning threshold of gt_thr1
System should take action to implement system cooling
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
Got ltThr0 interrupt through ESM module
System at a temperature below the threshold of lt_thr0
System running at a safe temperature
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x9, intSrc 0x9
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
ESM Call back function called : instType 0x1, intType 0x1, grpChannel 0x0, index 0xa, intSrc 0xa
Take action
ESM instance #1, ESM interrupt type = High Priority ESM event
case 0 sucess
Use Case 0 completed: Input Event Trigger = Step completed successfully,
Starting Use Case 1
Got gtThr1 interrupt through ESM module
Crossed early warning threshold of gt_thr1
System should take action to implement system cooling
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
Got gtThr2 interrupt through ESM module
Crossed critical threshold of gt_thr2
System should take critical action to implement system cooling
ESM Call back function called : instType 0x1, intType 0x1, grpChannel 0x0, index 0xa, intSrc 0xa
Take action
ESM instance #1, ESM interrupt type = High Priority ESM event
Got gtThr1 interrupt through ESM module
Crossed early warning threshold of gt_thr1
System should take action to implement system cooling
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
Got ltThr0 interrupt through ESM module
System at a temperature below the threshold of lt_thr0
System running at a safe temperature
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x9, intSrc 0x9
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
Use Case 1 completed: Input Event Trigger = Step completed successfully,
ESM Example Application summary
-------------------------------
Completed 2 Test Cases
Received 2 High Priority Interrupts
Received 5 Low Priority Interrupts
Test Case Event Log
------------------
Test Case 0: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 0: ESM Call back function called : grpChannel 0x0, index 0x9, intSrc 0x9
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 0: ESM Call back function called : grpChannel 0x0, index 0xa, intSrc 0xa
ESM instance #1, ESM interrupt type = High Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x0, index 0xa, intSrc 0xa
ESM instance #1, ESM interrupt type = High Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x9, intSrc 0x9
ESM instance #1, ESM interrupt type = Low Priority ESM event
VTM Example Application: Complete
All Use cases have passed.
main.c:531:vtm_example_app:PASS
-----------------------
1 Tests 0 Failures 0 Ignored