9.5. Developing Ethernet based applications with Linux + RTOS¶
9.5.1. Introduction¶
Common Port Switch (CPSW) provides Ethernet packet communication for the device. The total ports includes the following:
Internal Host Port which provides the packet streaming interface to the device cores
External MAC Port supporting the following:
Reduced Media Independent Interface (RMII)
Reduced Gigabit Media Independent Interface (RGMII)
Note that the MII modes supported vary based on device variant, please refer to the device’s TRM for the MII modes supported for each CPSW instance..
J721S2 has 2 instances
2-port (CPSW2G) in MCU domain (MCU_CPSW0)
2-port (CPSW2G) in Main domain (CPSW2)
Note
CPSW instance is commonly referred with number of ports suffixed to the CPSW. 2 port instances are referred to as CPSW2G.
9.5.2. CPSW Support Software¶
Enet LLD is low level driver residing in the PDK. It supports both CPSW2G instances in the SoC and provides HAL layer for higher level stacks.
TCP/IP Stack - Open source lwIP stack.
lwIP network interface driver (lwipif) is adaptation layer connecting Enet LLD to lwIP stack. This lwIP adaptation layer is part of Enet LLD and supports both CPSW2G instances with lwIP TCP/IP applications.
PTP Stack - PDK includes a test PTP stack used mainly to validate and demonstrate time synchronization integration with CPSW.
Note that this is not a production stack.
The scope of this developer note is to point to various documentation and source code resources available within the SDK (RTOS) to understand and use CPSW2G using Enet LLD in an user application.
9.5.3. Documentation References¶
SDK Component |
Documentation |
Description |
Section |
|---|---|---|---|
PDK |
Enet API guide |
Enet Driver |
|
PDK |
Enet Module User’s Guide - driver, examples |
Full document |
|
PDK |
Enet Integration Guide - further details about Enet LLD initialization |
Full document |
|
PDK |
lwIP network interface User’s Guide and Migration Guide |
Full document |
|
PDK |
PHY integration guide - to help integrating new PHY with Enet LLD |
Implementing a New PHY Driver |
|
PDK |
Link Configuration Guidelines |
Link Configuration Guidelines |
9.5.4. Source Code References¶
9.5.4.1. Enet LLD¶
SDK Component |
File / Folder |
Description |
|---|---|---|
PDK |
pdk/packages/ti/drv/enet/enet.h |
Enet LLD interface for both CPSW2G instances |
PDK |
pdk/packages/ti/drv/enet/include/phy/enetphy.h |
PHY LLD driver interface |
PDK |
pdk/packages/ti/drv/enet/lwipif/inc/lwipif2enet_appif.h |
App interface of the Enet-based lwIP network interface driver |
PDK |
pdk/packages/ti/drv/board/ |
Board drivers for GESI board |
9.5.4.2. lwIP¶
SDK Component |
File / Folder |
Description |
|---|---|---|
PDK |
pdk/packages/ti/transport/lwip/lwip-stack/src/include |
lwIP TCP/IP header files |
PDK |
pdk/packages/ti/transport/lwip/lwip-contrib/apps |
lwIP contrib application header files |
9.5.4.3. Example applications¶
SDK Component |
File / Folder |
Decription |
|---|---|---|
PDK |
pdk/packages/ti/drv/enet/examples/enet_loopback_test |
MCU CPSW2G internal loopback example mcu1_0, and Main CPSW2G on mcu2_0 |
PDK |
pdk/packages/ti/drv/enet/examples/enet_lwip_example |
lwIP integration example for MCU CPSW2G on mcu1_0 and Main CPSW2G on mcu2_0 |
The MAC port allocation in TI J721S2 EVM is as follows:
MCU CPSW2G - use the Ethernet port located in the J7X Common Processor Board labeled as MCU_ENET.
Main CPSW2G - use the Ethernet port located in the GESI board labeled as PRG0_RGMII1_B.
Make sure that the correct port is used when running the Enet LLD example applications.
9.5.5. Getting started on CPSW¶
Refer to Enet module documentation [LINK] for information about Enet LLD key APIs and the Examples section for available examples on this platform.
Refer to Enet LLD integration guide [LINK] for a further details about the initialization of an Ethernet peripheral via Enet LLD.
9.5.5.1. Configuring Ethernet port mode¶
Based on your board configuration, port can be in RMII, RGMII etc. mode. You need to do below to configure port in required mode.
Configure port ENET control to required mode using board library.
Configure CPSW interface.
For RMII, it should be configured to below:
interface->layerType = ENET_MAC_LAYER_MII; interface->sublayerType = ENET_MAC_SUBLAYER_REDUCED; interface->variantType = ENET_MAC_VARIANT_NONE;
For RGMII, it should be configured to below:
interface->layerType = ENET_MAC_LAYER_GMII; interface->sublayerType = ENET_MAC_SUBLAYER_REDUCED; interface->variantType = ENET_MAC_VARIANT_NONE;
9.5.5.2. Run Enet loopback example¶
We recommend running Enet loopback example first as this doesn’t have any dependency on board/EVM set up
See PDK user guide [LINK], section Build Steps for build steps
9.5.5.3. Run Enet lwIP example (TCP/IP example)¶
Once loopback example is run, you can run enet_lwip_example which uses lwIP stack for TCP/IP applications.
You need to connect EVM to PC running DHCP server. You should see IP printed on UART after running the example. The PDK Enet examples uses UART based on core it is running. Refer to PDK documentation for core-to-UART mapping. If you want to use static IP configuration, edit enet_lwip_example/lwipcfg.h to enable static IP.
You can ping to board using this IP address
You can also run iperf2 test (Enet LLD app is server, external PC is client).
9.5.5.4. Integrate new PHY in Enet¶
You need to add new PHY driver if existing PHY drivers present in enet/src/phy/* does not support PHY present on your Board.
Refer to PHY integration guide [LINK] which has details for adding support for new PHY in Enet LLD.
9.5.5.5. Modify the examples to support your board configuration¶
Modify examples to change PHY address, speed (10M/100M/1G etc.) setting, mode (RMII/RGMII etc.) settings.
Rebuild the example and run on your board. You should be able to see data transfer happening.