SDL Release Notes
Table of Contents
Introduction
This release notes provides important information that will assist you in using the SDL software package for the J721S2 family of devices. This document provides the product information and known issues that are specific to the SDL software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Defects. Also please check Upgrade and Compatibility for backward compatibility
What’s New
- Bug fixes
- R5 ECC cache example for performing double error detection (DED) for MCUR5F0
- ESM Error Pin PWM Mode Support.
- SDL PBIST Positive test include Reading of PBIST_PAGE Register.
Supported Modules
SDL support for the following modules are available:
- R5F PMU, MPU, RAT and VIM
- ESM
- PBIST
- LBIST
- POK
- VTM
- TOG
- ECC
- RTI
- R5F CCM
- DCC
- MCRC
- ROM CHECKSUM
Safety Examples for the following modules are provided:
- ESM
- POK
- VTM
- MTOG
- STOG
- DCC
- RTI
- ECC
- BIST
- ROM CHECKSUM
Upgrade and Compatibility
None
Supported Devices
- Platform: J721S2
Fixed Defects
| ID | Summary |
|---|---|
| PROC_SDL-9027 | J721s2: Power-off for DSS controller is failing between negative and positive tests |
| PROC_SDL-8685 | Multiple error callbacks received for one error injection for one ramId in the ecc_func_app |
| PROC_SDL-8943 | SDL application does not work with safertos BUILD_OS_TYPE |
| PROC_SDL-9176 | errSrc not defined in ecc_func.c |
| PROC_SDL-7653 | SDL Diagnostic Mapping XLS - missing instances |
Open Defects
| ID | Summary |
|---|---|
| PROC_SDL-8248 | SDL ECC error injection test for PCIE aggregators failure |
| PROC_SDL-7360 | j721s2: SDL_MCU_SA3_SS0_SA3SS_AM62_DMSS_ECCAGGR is defined but not used in ECC |
| PROC_SDL-8258 | SDL ECC error injection test for DSS ECC aggregators failure |
| PROC_SDL-8286 | SDL ECC error injection test for I3C ECC aggregators failure |
| PROC_SDL-8261 | ECC: Firewall related aggregators failures |
Migration Information
None.
Tool Chain Information
- Component: TI ARM R5F Clang Compiler tools
- Version: 4.0.1 LTS