|
PDK API Guide for J721S2
|
Go to the documentation of this file. 46 #ifndef PMIC_GPIO_LP8764X_H_ 47 #define PMIC_GPIO_LP8764X_H_ 66 #define PMIC_LP8764X_GPIO1_PIN (1U) 67 #define PMIC_LP8764X_GPIO2_PIN (2U) 68 #define PMIC_LP8764X_GPIO3_PIN (3U) 69 #define PMIC_LP8764X_GPIO4_PIN (4U) 70 #define PMIC_LP8764X_GPIO5_PIN (5U) 71 #define PMIC_LP8764X_GPIO6_PIN (6U) 72 #define PMIC_LP8764X_GPIO7_PIN (7U) 73 #define PMIC_LP8764X_GPIO8_PIN (8U) 74 #define PMIC_LP8764X_GPIO9_PIN (9U) 75 #define PMIC_LP8764X_GPIO10_PIN (10U) 86 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO (0U) 89 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO1_EN_DRV (1U) 92 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO2_SCL_I2C2 (1U) 95 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO3_SDA_I2C2 (1U) 98 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO4_ENABLE (1U) 101 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO5_SYNCCLKIN (1U) 104 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO6_GPIO7_NERR_MCU (1U) 107 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO8_SCLK_SPMI (1U) 110 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO9_SDATA_SPMI (1U) 113 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO10_NRSTOUT (1U) 116 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO1_GPIO10_NRSTOUT_SOC (2U) 119 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO2_CS_SPI (2U) 122 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO3_SDO_SPI (2U) 125 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO4_TRIG_WDOG (2U) 128 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO5_GPIO6_SYNCCLKOUT (2U) 131 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO7_REFOUT (2U) 134 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO8_VMON2 (2U) 137 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO9_PGOOD (2U) 140 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO1_GPIO6_PGOOD (3U) 143 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO2_TRIG_WDOG (3U) 146 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO4_BUCK1_VMON (3U) 149 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO5_NRSTOUT_SOC (3U) 152 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO7_VMON1 (3U) 155 #define PMIC_LP8764X_GPIO_PINFUNC_GPIO9_SYNCCLKIN (3U) 158 #define PMIC_LP8764X_GPIO_PINFUNC_NSLEEP1 (4U) 161 #define PMIC_LP8764X_GPIO_PINFUNC_NSLEEP2 (5U) 164 #define PMIC_LP8764X_GPIO_PINFUNC_WKUP1 (6U) 167 #define PMIC_LP8764X_GPIO_PINFUNC_WKUP2 (7U)