86 #if defined(MCU_PLUS_SDK) && !defined(QNX) 87 #if defined(HOST_EMULATION) 88 #include <drivers/dmautils/udma_standalone/udma.h> 90 #include <drivers/udma.h> 91 #include <drivers/udma/udma_priv.h> 94 #include <ti/drv/udma/udma.h> 97 #if !defined(SOC_AM62A) 126 #if !(defined(SOC_AM62A) || defined(SOC_J722S)) 127 #if defined(SOC_J721S2) || defined(SOC_J784S4) || defined(SOC_J742S2) 135 int32_t appUdmaCsirxCsitxInit(
void);
143 int32_t appUdmaCsirxCsitxDeInit(
void);
int32_t appUdmaDeInit(void)
Performs de-initializations needed for UDMA.
void appUdmaInitPrmSetDefault(app_udma_init_prms_t *prm)
Sets default UDMA init parameters.
Udma_VirtToPhyFxn virtToPhyFxn
Definition: app_udma.h:112
void * appUdmaCsirxCsitxGetObj(void)
Provides global handle to UDMA Obj BCDMA instance Required for CSIRX/CSITX on J721S2.
int32_t appUdmaTest(void)
DMA copy test function.
UDMA init parameters.
Definition: app_udma.h:110
int32_t appUdmaInit(const app_udma_init_prms_t *prms)
Performs initializations needed for UDMA.
void * appUdmaGetObj(void)
Provides global handle to UDMA Obj.