void Can_IntISR_Function(Can_ControllerInstance CanInstanceID, uint32 baseAddr)
This function is the ISR for CAN controller 0/INT 0.
Can_ControllerInstance
Can Controller Instances enum.
Definition: Can_Cfg.h:389
This file contains interface header for CAN MCAL driver.
This file contains generated pre compile configuration file for CAN MCAL driver.