34 #ifndef MATHLIB_SINH_H_
35 #define MATHLIB_SINH_H_
43 #include "../common/MATHLIB_types.h"
MATHLIB_STATUS MATHLIB_sinh(size_t length, T *pSrc, T *pDst)
Performs the elementwise hyperbolic sine of an input vector. Function can be overloaded with float po...
MATHLIB_STATUS MATHLIB_sinh_sp(size_t length, float *pSrc, float *pDst)
This function is the C interface for MATHLIB_sinh. Function accepts float pointers.
MATHLIB_STATUS_NAME
The enumeration of all status codes.