34 #ifndef MATHLIB_SIN_H_
35 #define MATHLIB_SIN_H_
43 #include "../common/MATHLIB_types.h"
MATHLIB_STATUS MATHLIB_sin_sp(size_t length, float *pSrc, float *pDst)
This function is the C interface for MATHLIB_sin. Function accepts float pointers.
MATHLIB_STATUS MATHLIB_sin(size_t length, T *pSrc, T *pDst)
Performs the elementwise sine of an input vector. Function can be overloaded with float and double po...
MATHLIB_STATUS MATHLIB_sin_dp(size_t length, double *pSrc, double *pDst)
This function is the C interface for MATHLIB_sin. Function accepts double pointers.
MATHLIB_STATUS_NAME
The enumeration of all status codes.