34 #ifndef MATHLIB_EXP2_H_
35 #define MATHLIB_EXP2_H_
43 #include "../common/MATHLIB_types.h"
MATHLIB_STATUS MATHLIB_exp2(size_t length, T *pSrc, T *pDst)
Performs the elementwise 2^x for all x in the input vector. Function can be overloaded with float poi...
MATHLIB_STATUS MATHLIB_exp2_sp(size_t length, float *pSrc, float *pDst)
This function is the C interface for MATHLIB_exp2. Function accepts float pointers.
MATHLIB_STATUS_NAME
The enumeration of all status codes.