63 #ifndef HWA_VPAC3L_VISS_H_ 64 #define HWA_VPAC3L_VISS_H_ 67 #include <VX/vx_kernels.h> 81 #define TIVX_VPAC_VISS_MAX_OUTPUTS (6U) 83 #define TIVX_VPAC_VISS_FCP_NUM_INSTANCES (1U) 86 #define TIVX_VPAC_VISS_IR_DISABLE (0U) 88 #define TIVX_VPAC_VISS_IR_ENABLE (1U) 91 #define TIVX_VPAC_VISS_BAYER_DISABLE (0U) 93 #define TIVX_VPAC_VISS_BAYER_ENABLE (1U) 107 uint32_t sensor_dcc_id;
116 uint32_t fcp1_config;
140 uint32_t output_fcp_mapping[5];
152 uint32_t bypass_nsf4;
156 uint32_t bypass_glbce;
187 uint32_t h3a_aewb_af_mode;
226 uint32_t enable_error_events;
387 vx_user_data_object configuration,
388 vx_user_data_object ae_awb_result,
389 vx_user_data_object dcc_buf,
396 vx_user_data_object h3a_output,
397 vx_distribution histogram0,
398 vx_distribution histogram1,
399 vx_distribution raw_histogram);
uint32_t enable_bayer_op
Definition: hwa_vpac_viss3l.h:134
uint32_t enable_ir_op
Definition: hwa_vpac_viss3l.h:126
The Flex Color Processing (FCP) data structure used in the tivx_vpac_viss_params_t structure for prog...
Definition: hwa_vpac_viss_fcp.h:181
uint32_t bypass_pcid
Definition: hwa_vpac_viss3l.h:160
VX_API_ENTRY vx_node VX_API_CALL tivxVpacVissNode(vx_graph graph, vx_user_data_object configuration, vx_user_data_object ae_awb_result, vx_user_data_object dcc_buf, tivx_raw_image raw, vx_image output0, vx_image output1, vx_image output2, vx_image output3, vx_image output4, vx_user_data_object h3a_output, vx_distribution histogram0, vx_distribution histogram1, vx_distribution raw_histogram)
[Graph] Creates a VPAC_VISS Node.
#define TIVX_VPAC_VISS_MAX_OUTPUTS
Max Output Channels.
Definition: hwa_vpac_viss3l.h:81
uint32_t ir_output
Definition: hwa_vpac_viss3l.h:130
#define TIVX_VPAC_VISS_FCP_NUM_INSTANCES
Definition: hwa_vpac_viss3l.h:83
The configuration data structure used by the TIVX_KERNEL_VISS kernel.
Definition: hwa_vpac_viss1.h:93
Definition: hwa_vpac_viss1.h:201