81 #ifndef FFTLIB_IFFT1D_I32FC_C32FC_O32FC_H_
82 #define FFTLIB_IFFT1D_I32FC_C32FC_O32FC_H_ 1
84 #include "../../common/FFTLIB_types.h"
103 #define FFTLIB_FFT1D_I32FC_C32FC_O32FC_PBLOCK_SIZE (11 * SE_PARAM_SIZE)
FFTLIB_STATUS_NAME
The enumeration of all status codes.
float FFTLIB_F32
Single precision floating point.
FFTLIB_STATUS FFTLIB_ifft1d_i32fc_c32fc_o32fc_checkParams(FFTLIB_F32 *pX, FFTLIB_bufParams1D_t *bufParamsX, FFTLIB_F32 *pW, FFTLIB_bufParams1D_t *bufParamsW, FFTLIB_F32 *pY, FFTLIB_bufParams1D_t *bufParamsY, void *pBlock)
This function checks the validity of the parameters passed to FFTLIB_ifft1d_i32fc_c32fc_o32fc_init an...
FFTLIB_STATUS FFTLIB_ifft1d_i32fc_c32fc_o32fc_init(FFTLIB_F32 *pX, FFTLIB_bufParams1D_t *bufParamsX, FFTLIB_F32 *pW, FFTLIB_bufParams1D_t *bufParamsW, FFTLIB_F32 *pY, FFTLIB_bufParams1D_t *bufParamsY, void *pBlock)
This function should be called before the FFTLIB_ifft1d_i32fc_c32fc_o32fc_kernel function is called....
FFTLIB_STATUS FFTLIB_ifft1d_i32fc_c32fc_o32fc_kernel(FFTLIB_F32 *pX, FFTLIB_bufParams1D_t *bufParamsX, FFTLIB_F32 *pW, FFTLIB_bufParams1D_t *bufParamsW, FFTLIB_F32 *pY, FFTLIB_bufParams1D_t *bufParamsY, void *pBlock)
This function is the main kernel compute function.
A structure for a 1 dimensional buffer descriptor.