TIOVX Release Notes
Version: 09.02.00
Contents
- Introduction
- Licensing
- Getting Started
- Documentation
- What's New
- Upgrade and Compatibility Information
- Device Support
- Validation Information
- Fixed Issues
- Known Issues
- Change Requests
- Technical Support
- Package Versioning
Introduction
The TIOVX package consists of the Texas Instruments OpenVX conformant implementation for Jacinto7 platform
Licensing
The licensing information of this library, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. A complete manifest along with export control information is detailed here [HTML].
Getting Started
The TIOVX User Guide [HTML] provides the documentation and references necessary to begin development on TI's platforms using TIOVX.
Documentation
Refer to following documentation for further details:
TIOVX User Guide | Build instructions, API Guide, tutorials, tool documentation, etc | [HTML] |
Test Reports | Conformance test reports, TI platform test reports | [XLSX] |
Software Manifest | Licenses, terms of use | [HTML] |
Static Analysis Report | C and C++ Taxonomy Report | [XLSX] |
Bidirectional Traceability Report | Traceability reports of MR to FR to Test | [XLSX] |
FMEA | Failure modes and effects analysis of TIOVX framework, platform and utils layers | Available upon request. (This will be publicly available when TIOVX safety is complete in SDK 10.1) |
What's New
ID | Summary |
---|---|
TIOVX-56 | Coding: Framework shall be MISRAC 2012 Compliant |
TIOVX-1540 | TIOVX shall support Khronos Safe Casts Extension |
TIOVX-1497 | TIOVX shall support Khronos Bidirectional Parameters Extension |
TIOVX-1479 | TIOVX buffer allocator shall support a heap with cache write through policy |
Upgrade and Compatibility Information
File | Change description | User application change required | User application recompile required | include\TI\tivx_obj_desc.h | The TIVX_IMAGE_MAX_PLANES value has increased from "3" to "4" | NO | YES |
include\TI\soc\tivx_config*.h | Several of the max values have increased to support various use cases | NO | YES |
include\TI\tivx_target_kernel.h | The tivxPlatformGetDmaObj has been deprecated in favor of appUdmaGetObj in app_utils | YES | YES |
Device Support
SoC | Target (OS) | Test Plaform |
---|---|---|
J721S2 | x86_64 (Linux) | x86_64 Linux with Ubuntu 22.04 |
J721S2 | R5F, C7x running FreeRTOS or SafeRTOS A72 running Linux Kernel v6.1 or QNX |
J721S2 EVM |
Validation Information
This release was built and validated using the following tools:
Build Tools (included in Processor SDK RTOS):
- C7000 Code Generation Tools version: 4.1.0.LTS
- GCC ARM Linux Code Generation Tools version: 11.3
- TI ARM LLVM Code Generation Tools version: 3.2.1.LTS
Dependencies (included in Processor SDK RTOS):
- VXLIB version: 1.1.7.0
- Processor SDK RTOS version: 09.02.00
Dependencies (NOT included in Processor SDK RTOS):
- GCC: 5.11.0
- libpng: 1.2
Fixed Issues
ID | Summary |
---|---|
TIOVX-1559 | Error in graph stream release logic |
TIOVX-1518 | Supported kernels table renders incorrectly |
TIOVX-1458 | Documentation: Resource stats apis are not grouped together |
TIOVX-1456 | Documentation: obj_desc count table within vx_log_resource is core/process specific |
TIOVX-1455 | SPINLOCK implementation in TIOVX deviated from the TRM suggestions. |
TIOVX-1450 | Accessing object descriptor of image on unsuccesful creation of image. |
TIOVX-1428 | Conformance test case failure due to status check given for ownReleaseReferenceInt function call in vxReleaseKernel API |
TIOVX-1338 | [CSITX]: No clean exit when buffers are not enqueued |
Known Issues
ID | Summary |
---|---|
TIOVX-1453 | Linux: APIs like vxSwapImageHandle, tivxReferenceImport and export handles does not consider dma_buf_fd |
TIOVX-1432 | subset of tivxGraphPipeline.ReplicateImage2 test cases fail when run via ssh |
TIOVX-1428 | Conformance test case failure due to status check given for ownReleaseReferenceInt function call in vxReleaseKernel API |
TIOVX-1344 | Display conformance tests giving wrong output for ADAS image (J721E, J721S2, J784S4) |
TIOVX-1338 | [CSITX]: No clean exit when buffers are not enqueued |
TIOVX-1309 | Canny robustness test failing on PC emulation with full conformance test suite |
TIOVX-1297 | vxScaleImageNode Upsampling output is not as expected for fractional scaling |
TIOVX-1238 | Frame Freeze in QNX when LDC node, Mosaic node and a Display node added to SRV demo |
TIOVX-1023 | tivxGraphPipeline.MaxDataRef disabled due to failure caused by boundary condition |
TIOVX-823 | TIOVX delay parameters with pipelining result in serialization of nodes |
TIOVX-569 | Bmp utils do not work for loading RGBX images |
VXLIB-371 | Multiply iS16 iS16 oS16 with 1/255 as scaling factor fails for X86 target |
TIOVX-1238 | Frame Freeze in QNX when LDC node, Mosaic node and a Display node added to SRV demo. Patch attached here can be used to fix issue |
ADASVISION-5758 | Enable en_out_ldc_write causes freeze in Multi Cam Demo. Patch attached here can be used to fix issue |
Change Requests
ID | Headline | Original Fix Version | New Fix Version |
---|---|---|---|
JACINTOREQ-7507 | Defer benchmark numbers on IPC with OpenVX overhead on J7 platforms to 10.1 release | 09.02.00 | 10.01.00 |
Technical Support
For technical support and additional assistance, contact local TI Field Application Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]
. The table below provides a descriptive reference regarding package version numbering.
Digit | Meaning | Description |
---|---|---|
1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
Copyright 2023, Texas Instruments Incorporated