37 #include <tistdtypes.h> 38 #include <sdl_types.h> 40 #if defined (SOC_J721E) 41 #include <include/soc/j721e/sdlr_soc_baseaddress.h> 42 #include <src/sdl/rti/soc/j721e/sdl_soc_rti.h> 45 #if defined (SOC_J7200) 46 #include <include/soc/j7200/sdlr_soc_baseaddress.h> 47 #include <src/sdl/rti/soc/j7200/sdl_soc_rti.h> 50 #if defined (SOC_J721S2) 51 #include <include/soc/j721s2/sdlr_soc_baseaddress.h> 55 #if defined (SOC_J784S4) 56 #include <include/soc/j784s4/sdlr_soc_baseaddress.h> 57 #include <src/sdl/rti/soc/j784s4/sdl_soc_rti.h> 231 #define RTI_DWWD_WINDOWSIZE_100_PERCENT (RTI_RTIDWWDSIZECTRL_DWWDSIZE_100_PERCENT) 233 #define RTI_DWWD_WINDOWSIZE_50_PERCENT (RTI_RTIDWWDSIZECTRL_DWWDSIZE_50_PERCENT) 235 #define RTI_DWWD_WINDOWSIZE_25_PERCENT (RTI_RTIDWWDSIZECTRL_DWWDSIZE_25_PERCENT) 237 #define RTI_DWWD_WINDOWSIZE_12_5_PERCENT (RTI_RTIDWWDSIZECTRL_DWWDSIZE_12_5_PERCENT) 239 #define RTI_DWWD_WINDOWSIZE_6_25_PERCENT (RTI_RTIDWWDSIZECTRL_DWWDSIZE_6_25_PERCENT) 241 #define RTI_DWWD_WINDOWSIZE_3_125_PERCENT (RTI_RTIDWWDSIZECTRL_DWWDSIZE_3_125_PERCENT) 265 #define RTI_DWWD_REACTION_GENERATE_RESET (RTI_RTIDWWDRXNCTRL_DWWDRXN_RESET) 267 #define RTI_DWWD_REACTION_GENERATE_NMI (RTI_RTIDWWDRXNCTRL_DWWDRXN_INTERRUPT) 272 #define RTI_DWWD_REACTION_INVALID (0x46U) 279 #define RTI_DWWD_STATUS_KEY_SEQ_VIOLATION (RTI_RTIWDSTATUS_KEYST_MASK) 281 #define RTI_DWWD_STATUS_TIME_WINDOW_VIOLATION (RTI_RTIWDSTATUS_DWWD_ST_MASK) 283 #define RTI_DWWD_STATUS_ENDTIME_WINDOW_VIOLATION (RTI_RTIWDSTATUS_END_TIME_VIOL_MASK) 285 #define RTI_DWWD_STATUS_STARTTIME_WINDOW_VIOLATION (RTI_RTIWDSTATUS_START_TIME_VIOL_MASK) 287 #define RTI_DWWD_STATUS_LAST_RESET (RTI_RTIWDSTATUS_DWDST_MASK) 311 #define RTI_RTIDWDCTRL (0x90U) 312 #define RTI_RTIDWDPRLD (0x94U) 313 #define RTI_RTIWDSTATUS (0x98U) 314 #define RTI_RTIWDKEY (0x9cU) 316 #define RTI_RTIDWWDRXNCTRL (0xa4U) 317 #define RTI_RTIDWWDSIZECTRL (0xa8U) 318 #define RTI_RTIDWDCNTR (0xa0U) 319 #define RTI_COMP0 (0x50U) 321 #define STATUS_VLD (1U) 329 #define RTI_RTIDWDCTRL_DWDCTRL_ENABLE (0xA98559DAU) 331 #define RTI_DWWDPRLD_MULTIPLIER_SHIFT (13U) 333 #define RTI_RTIDWDPRLD_INVALID (0xFFFFFFU) 334 #define RTI_RTIDWDPRLD_DWDPRLD_SHIFT (0U) 335 #define RTI_RTIDWDPRLD_DWDPRLD_MASK (0x00000fffU) 336 #define RTI_RTIDWDPRLD_DWDPRLD_MAX (0x0FFFU) 338 #define RTI_RTIDWDCNTR_DWDCNTR_15_0_SHIFT (0U) 339 #define RTI_RTIDWDCNTR_DWDCNTR_15_0_MASK (0x0000ffffU) 341 #define RTI_RTIDWDCNTR_DWDCNTR_24_16_SHIFT (16U) 342 #define RTI_RTIDWDCNTR_DWDCNTR_24_16_MASK (0x01ff0000U) 344 #define RTI_RTIWDSTATUS_DWDST_SHIFT (1U) 345 #define RTI_RTIWDSTATUS_DWDST_MASK (0x00000002U) 347 #define RTI_RTIWDSTATUS_DWWD_ST_SHIFT (5U) 348 #define RTI_RTIWDSTATUS_DWWD_ST_MASK (0x00000020U) 350 #define RTI_RTIWDKEY_WDKEY_SHIFT (0U) 351 #define RTI_RTIWDKEY_WDKEY_MASK (0x0000ffffU) 352 #define RTI_RTIWDKEY_WDKEY_FIRST_WRITE (0x0000E51AU) 353 #define RTI_RTIWDKEY_WDKEY_SECOND_WRITE (0x0000A35CU) 355 #define RTI_RTIDWWDRXNCTRL_DWWDRXN_SHIFT (0U) 356 #define RTI_RTIDWWDRXNCTRL_DWWDRXN_MASK (0x0000000fU) 357 #define RTI_RTIDWWDRXNCTRL_DWWDRXN_RESET (0x5U) 358 #define RTI_RTIDWWDRXNCTRL_DWWDRXN_INTERRUPT (0xAU) 360 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_INVALID (0U) 361 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_SHIFT (0U) 362 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_MASK (0x00ffffffU) 363 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_100_PERCENT (0x00000005U) 364 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_100_PERCENT_SHIFT (0x0) 365 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_50_PERCENT (0x00000050U) 366 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_50_PERCENT_SHIFT (0x1) 367 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_25_PERCENT (0x00000500U) 368 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_25_PERCENT_SHIFT (0x2) 369 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_12_5_PERCENT (0x00005000U) 370 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_12_5_PERCENT_SHIFT (0x3) 371 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_6_25_PERCENT (0x00050000U) 372 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_6_25_PERCENT_SHIFT (0x4) 373 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_3_125_PERCENT (0x00500000U) 374 #define RTI_RTIDWWDSIZECTRL_DWWDSIZE_3_125_PERCENT_SHIFT (0x5) 385 RTI_RTIDWWDSIZECTRL_DWWDSIZE,
387 sdlResult = SDL_PASS;
404 RTI_RTIDWWDRXNCTRL_DWWDRXN,
406 sdlResult = SDL_PASS;
417 uint32_t dwwdReaction;
421 RTI_RTIDWWDRXNCTRL_DWWDRXN);
static uint32_t SDL_RTI_readReaction(uint32_t baseAddr)
Definition: sdl_ip_rti.h:415
List of Config Parameters for RTI DWWD.
Definition: sdl_ip_rti.h:129
uint32_t RTI_Status_t
type to report the DWWD status.
Definition: sdl_ip_rti.h:300
uint32_t SDL_RTI_dwwdWindowSize
Definition: sdl_ip_rti.h:133
int32_t SDL_RTI_chkWindowSize(uint32_t dwwdWindowSize)
This API will check the Window Size for DWWD.
int32_t SDL_RTI_setPreload(uint32_t baseAddr, uint32_t dwwdPreloadVal)
Set DWWD preload value. From this value down counter starts down counting.
static int32_t SDL_RTI_writeWinSz(uint32_t baseAddr, uint32_t dwwdWindowSize)
Definition: sdl_ip_rti.h:380
uint32_t SDL_RTI_dwwdReaction
Definition: sdl_ip_rti.h:135
#define RTI_RTIDWWDRXNCTRL
Definition: sdl_ip_rti.h:316
uint32_t RTI_WindowSize_t
type to select the DWWD window size.
Definition: sdl_ip_rti.h:252
uint32_t SDL_RTI_dwwdPreloadVal
Definition: sdl_ip_rti.h:131
static int32_t SDL_RTI_writeReaction(uint32_t baseAddr, uint32_t dwwdReaction)
Definition: sdl_ip_rti.h:396
uint32_t RTI_DWDCTRL
Definition: sdl_ip_rti.h:115
uint32_t RTI_DWDPRLD
Definition: sdl_ip_rti.h:117
uint32_t RTI_WWDSIZECTRL
Definition: sdl_ip_rti.h:121
int32_t SDL_RTI_getWindowSize(uint32_t baseAddr, uint32_t *pWinSize)
This API will return current configured Window Size.
uint32_t RTI_WWDRXNCTRL
Definition: sdl_ip_rti.h:119
#define RTI_RTIDWWDSIZECTRL
Definition: sdl_ip_rti.h:317
List of Static Registers for RTI DWWD.
Definition: sdl_ip_rti.h:112
int32_t SDL_RTI_getPreload(uint32_t baseAddr, uint32_t *pPreloadVal)
This API will return current configured Preload value.
int32_t SDL_RTI_chkReaction(uint32_t dwwdReaction)
This API will check the reaction to perform when error is detected from DWWD.