This example shows how to write an OpenVx application which integrates the camera pipeline to TIDL based Object Detection pipeline. The demo is validated on Pelee network available at, https://github.com/Robert-JunWang/Pelee. Raw pixels from sensor is captured via CSI2Rx and sent to VISS for image processing. The resulting image is written in NV12 format which is then sent to LDC for fish-eye rectification. The rectified image is scaled using MSC to produce a DL resolution of 1024x512 as required by the Pelee network. As a pre-processing step, the scaled NV12 resolution is converted to RGB format and padded as required on C66x_1 DSP. The pre-processed input is given to TIDL running on C7x DSP for inference. As a post-processing step, the TIDL output is read and top detections are rendered as 2D boxes on the provided image on C66x_2 DSP. The final output is blended with system performance statistics and displayed on a 1920x1080 screen.
| Platform | Linux x86_64 | Linux+RTOS mode | QNX+RTOS mode | SoC |
|---|---|---|---|---|
| Support | NO | YES | YES | J721e / J721S2 / J784S4 |
Note: On J721S2 and J784S4, the algorithms running on C66_1 and C66_2 have been recompiled and are running on the standalone C7X.
Shown below is a example for running object detection on 4 IMX390 2MP cameras