5.5.6.1.4.1. Enet TSN Example¶
5.5.6.1.4.1.1. Makefile¶
For an example of the app makefile, please refer to <enet>/examples/enet_tsn_example/makefile.
There are some important notes to consider:
To include TSN components, add the following macros:
INCLUDE_INTERNAL_INTERFACES += tsn_gptp tsn_combase tsn_unibase COMP_LIST_COMMON += tsn_combase tsn_unibase tsn_gptp
Ensure that the
tsninit.cfile is included in the app’s source:SRCS_COMMON += main.c tsninit.c
If the log task is used, define the
TSN_USE_LOG_BUFFERmacro:CFLAGS_LOCAL_COMMON += -DTSN_USE_LOG_BUFFER=1
Include the
tsn_tilld_include.hat the beginning to ensure the correct inclusion of combase headers:CFLAGS_LOCAL_COMMON += -include $(PDK_TSN_COMP_PATH)/tsn-stack/tsn_tilld_include.h
5.5.6.1.4.1.2. Build Enet TSN example¶
Navigate to the <pdk>/packages/ti/build directory:
$ cd <pdk>/packages/ti/build
Build the TSN modules (tsn_unibase, tsn_combase, tsn_gptp):
$ make tsn_unibase tsn_combase tsn_gptp
To clean the build and remove generated files:
$ make tsn_unibase_clean tsn_combase_clean tsn_gptp_clean
You can specify the build mode as either release or debug. By default, the release mode is built. To build in debug mode, use the
BUILD_PROFILE=debugoption:$ make tsn_unibase tsn_combase tsn_gptp BUILD_PROFILE=debug
If you want to build with C++ compiling rules, use the
CPLUSPLUS_BUILD=yesoption:$ make tsn_unibase tsn_combase tsn_gptp CPLUSPLUS_BUILD=yes
To build the TSN example app in the PDK, use the following command:
$ make enet_tsn_example_freertos CORE=mcu2_0
The example app binary file can be found at the following location:
<pdk>/packages/ti/binary/enet_tsn_example_freertos/bin/j7200_evm/enet_tsn_example_freertos_mcu2_0_release.xer5f
This command will build the TSN example app (
enet_tsn_example_freertos) using the FreeRTOS operating system and targeting the mcu2_0 core. Adjust the command according to your specific requirements, such as selecting a different operating system or core if needed.
5.5.6.1.4.1.3. Running Enet TSN example¶
Launch a CCS debug session, load and run
enet_tsn_example_freertos_mcu2_0_release.xer5fbinary file to the MAIN_Cortex_R5_0_0. Alternatively, the example application can be loaded using any other boot method such as MMC/SD.Logs will be printed in Main UART port 0. Below is an example of the log when gPTP works in slave mode:
========================== TSN App ========================== EnetBoard_setupPorts: 2 of 2 ports configurations found main: EnetBoard_setupPorts() done main: EnetApp_init() done tsnapp_task:gptp start done! CPU Load: 2% gptp_task: started. EnetMcm: CPSW_9G on MAIN NAVSS Mdio_open: MDIO manual mode enabled PHY 0 is alive PHY 4 is alive EnetPhy_bindDriver: PHY 0: OUI:080028 Model:29 Ver:00 <-> 'Dp83tg721' : OK EnetPhy_bindDriver: PHY 4: OUI:080028 Model:29 Ver:00 <-> 'Dp83tg721' : OK log_task: started. unibase-1.1.4-46b7374 INF:gptp:gptpnet_init:Open lldtsync OK! INF:gptp:000000-624234:domainIndex=0, GM changed old=00:00:00:00:00:00:00:00, new=70:FF:76:FF:FE:1D:9B:77 INF:gptp:set_phase_offsetGM:domainNumber=0, New adjustment(New GM?) Cpsw_handleLinkUp: Port 1: Link up: 1-Gbps Full-Duplex Cpsw_handleLinkUp: Port 2: Link up: 1-Gbps Full-Duplex MAC Port 1: link up MAC Port 2: link up INF:gptp:index=1 speed=1000, duplex=full, ptpdev=tilld0 INF:gptp:index=2 speed=1000, duplex=full, ptpdev=tilld1 ... INF:gptp:set_phase_offsetGM:domainNumber=0, New adjustment(New GM?) INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment, diff=686848947 WRN:gptp:gptpclock_setoffset64:clockIndex=1, domainNumber=0, can't set in the time. the result must be inaccurate INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=210489 INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=212961 INF:gptp:clock_master_sync_receive:computeGmRateRatio:domainNumber=0 unstable rate=19781ppb (timeleap_future) INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 232742ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=201161 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 339521ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=182536 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 373116ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=161714 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 368386ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=141167 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 345162ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=121872 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 314067ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=104701 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 280212ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=89613 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 249210ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=76477 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 220595ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=65129 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 194956ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=55384 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 172395ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=47051 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 152814ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=39952 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 135971ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=33854 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 121469ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=28696 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 108546ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=24363 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 98255ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=20682 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 89492ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=17551 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 81991ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=14889 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 75586ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=12627 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 70128ppb INF:gptp:set_phase_offsetGM:domainNumber=0, offset adjustment by Freq., diff=10710 INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 65499ppb INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 61563ppb INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 58249ppb INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 55383ppb ...
5.5.6.1.4.1.4. Verification¶
Single port
Connect a port to a Linux PC and run gptp2d from the PC.
The expected log from the slave side will be stable and reprinted like this:
INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 65499ppb
INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 61563ppb
INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 58249ppb
INF:gptp:domainNumber=0, clock_master_sync_receive:the master clock rate to 55383ppb
...
Instead of displaying the clock_master_sync_receive:... log, the following log
will be printed in the case of the master log:
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
CPU Load: 2%
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
CPU Load: 2%
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
CPU Load: 2%
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
...
Multiple ports
In this function, gPTP is operating as a switch. The availability of this feature is determined by the board configuration rather than the gPTP stack. If a board enables multiple MAC ports, the gPTP function should operate properly. To test this function, please connect two PCs to two ports of the EVM.
When the EVM board acts as the master, only the master log will be printed out, while the two PCs will print the slave log. On the other hand, if one of the PCs acts as the master, the slave log will be printed by the other PC and the EVM, while the master PC will print the master log.
To identify which machine is the master, please check the log:
INF:gptp:001809-750000:domainIndex=0, GM changed old=24:76:25:FF:FE:96:6C:41, new=70:FF:76:FF:FE:1D:9B:77
In this case, the machine with the source MAC address of 70:FF:76:FF:FE:1D:9B:77 is the master.