Vision Apps Release Notes
Version: 08.06.00
Contents
- Introduction
- Licensing
- Getting Started
- Documentation
- What's New
- Upgrade and Compatibility Information
- Device Support
- Validation Information
- Fixed Issues
- Open Defects
- Known Issues
- Change Requests
- Technical Support
- Package Versioning
Introduction
The Vision Apps package consists of ADAS, vision, deep learning, perception demos/applications for Jacinto 7 platform
To run the demos in vision apps, the companion Processor SDK Linux for Jacinto 7 also needs to be downloaded separately.
Licensing
Refer to Processor SDK RTOS manifest at top level [HTML]
Getting Started
The Vision Apps User Guide [HTML] provides the documentation and references necessary to begin development on TI's platforms using Vision Apps.
Documentation
Refer to following documentation for further details:
Vision Apps User Guide | Build instructions, API Guide | [HTML] |
Surround View Manual Calibration Tool | Instructions for Generating Calibration Binaries | [PDF] |
Release Notes Archive | Previous release notes | [FOLDER] |
What's New
New features in this release are highlighted in bold- OpenVX based demos for ADAS, Vision, deep learning applications
- Free RTOS and Safe RTOS C7x and R5F and Linux or QNX on A72
- Integrates all major PSDK RTOS and PSDK Linux SW components like TIDL, MMALIB, PDK, OpenVX, OpenGL, C7x algorithms, imaging/sensors, IPC, Linux, TI-RTOS, SPL/uboot.
- Integrates all major HW components like CSI2 camera, eDP/HDMI display, UART, I2C, SD card
- Deep Learning demos
- Image Classification demo
- File based
- Camera based
- Standalone Semantic Segmentation application
- File based
- Camera based
- Standalone Object Detection application
- File based
- Camera based
- Auto valet parking (AVP) demo
- semantic segmentation, Parking spot detect and Vehicle detect algorithms
- 1 channel, 3 algo mode
- 3 channel, 3 algo mode (combined network for parking spot and vehicle detect)
- 3 channel, 5 algo mode - combined network for parking spot and vehicle detect + Three task network for Semantic Segmentation, Motion Segmentation and Depth Estimation (AVP3 demo)
- DKAZE-based Visual Localization application
- Debug support for the ability to debug intermediate layer information from TIDL node
- Surround View demos
- 3D surround view using GPU on 4x 2MP 30fps live camera input
- 3D surround view calibration application
- ADAS/Vision demos
- Dense optical flow (DOF) demo
- Stereo disparity engine demo
- Single and multi camera CSI2RX + VISS + LDC + MSC + Display demo
- Multi channel codec demo utilizing CSI2RX + VISS + LDC + MSC + Display with Linux and QNX running on A72
- C7x algorithm offload demo (with DMA acceleration)
- CV Demos
- Structure from motion
- OpenVX target nodes
- image pre-processing (YUV 2 RGB) nodes for DL demos
- image post-processing and visualization nodes for deep learning, DOF, Stereo demos
- OpenGL nodes for surround view
- Multi-threading support in MSC mosaic node
- Profiling, logging and other utility APIs
- General stability, performance, documentation improvements
- All included MCU tasks are split between MCU2_0 (ETHFW, VPAC HWA) and MCU2_1 (DMPAC HWA), leaving MCU3_0 and MCU3_1 free on main island
Upgrade and Compatibility Information
File | Change description | User application change required | User application recompile required |
kernels_j7\include\TI\j7.h | This file is deprecated and removed in this SDK. | YES | YES |
Device Support
Refer Processor SDK RTOS release notes [HTML]
Validation Information
The tools used to validate this package are listed in top level user guide [HTML]
Fixed Issues
ID | Summary |
---|---|
ADASVISION-4198 | Partial failure observed for IPC test when MCU1_0 is enabled due to secure mode boot |
ADASVISION-5727 | 2A Node error handling of CPU ID is incorrect |
ADASVISION-5704 | J721S2: SAFERTOS: Instability observed on C7X |
ADASVISION-5399 | VPAC/DMPAC Func clock not enabled for j721s2 |
ADASVISION-5065 | OCMC RAM Init fails on MCU2-0 |
Open Defects
ID | Summary |
---|---|
ADASVISION-5791 | Memory leak observed when multicam codec demo is run on J721s2 |
ADASVISION-5789 | vx_app_load_test provides a lower load when given 100% load as input |
ADASVISION-5788 | L2_MEM shows 100% unused when tidl_od demo is run |
ADASVISION-5763 | MCU2_0 startups much more slower if its OS is SafeRTOS |
ADASVISION-5758 | Enable en_out_ldc_write cause freeze in Multi Cam Demo |
ADASVISION-5734 | App_multi_cam_codec decode framerate drops for more than 2 channels |
ADASVISION-5732 | eDP to HDMI adaptors failing on J721S2 QNX builds with SBL boot app |
ADASVISION-5727 | 2A Node error handling of CPU ID is incorrect |
ADASVISION-5673 | Permission issue can occur when running the vision apps script incorrectly |
ADASVISION-5531 | [NF]: Incorrect condition check when skip is enabled |
ADASVISION-5555 | SDE disparity artifacts on EVM |
ADASVISION-5393 | AVP4 freezes in first second of running on QNX |
ADASVISION-5100 | Peak DDR BW numbers seem too high for some demos |
ADASVISION-4923 | Frozen frame running OpenVX graphs back to back |
ADASVISION-4799 | Broadcast Mode Unreliable |
ADASVISION-4386 | QNX SBL debug binaries not working on R5F |
ADASVISION-4198 | Partial failure observed for IPC test when MCU1_0 is enabled due to secure mode boot |
ADASVISION-4039 | Frame drops in 8 camera, 30 fps demo |
Known Issues
ID | Summary | Workaround |
---|---|---|
ADASVISION-4345 | SteamFIFO overflow observed in long run > 6hrs when using D3 IMX390 CM cameras | Upgrade to D3 IMX390 RCM cameras |
Change Requests
ID | Headline | Original Fix Version | New Fix Version |
---|---|---|---|
JACINTOREQ-5018 | De-scope BAM enablement on J7 from 8.6 | 08.06.00 | 09.01.00 |
JACINTOREQ-5384 | Push Out Decode + Display MR's on J721S2 and J784S4 on QNX | 08.06.00 | 09.00.00 |
JACINTOREQ-5374 | Descope Orphaned FR's for J721E, J721S2, and J784S4 on QNX | 08.06.00 | DESCOPE |
Technical Support
For technical support and additional assistance, contact local TI Field Application Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]
. The table below provides a descriptive reference regarding package version numbering.
Digit | Meaning | Description |
---|---|---|
1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
Copyright 2020, Texas Instruments Incorporated