5.12. SPI¶
5.12.1. Introduction¶
SPI driver enables communication for general SPI, MCSPI (Multichannel SPI), QSPI (Quad SPI) and OSPI (Octal SPI) based peripherals on board through common API to application. MCSPI is a generic full-duplex interface supporting transmit and receive of data over SPI bus. QSPI/OSPI is a variant of SPI supports four/eight receive data lanes. Driver supports configuration for either single, dual, quad or octal data lines
5.12.1.1. Modes of Operation¶
Following modes of operations are supported:
SPI_MODE_BLOCKING SPI_transfer() API blocks code execution until transaction has completed. By default, SPI driver operates in blocking mode. This ensures only one SPI transaction operates at a given time. This mode is supported in both interrupt or non-interrupt configurations.
SPI_MODE_CALLBACK SPI_transfer() API returns without waiting for completion of transaction in this case. Callback function registered by application is invoked once transaction is complete.This mode is supported only in interrupt configuration.
5.12.2. Driver Configuration¶
5.12.2.1. Board Specific Configuration¶
All board specific configurations eg:enabling clock and pin-mux for SPI pins are required before calling any driver APIs.By default Board_Init() API supports all initialization sequence for TI supported EVMs. In addition it initializes UART instance for Console/STDIO.Refer PDK Board Support for additional details.Once board specific configuration is complete SPI_init() API should be called to initialize driver.
5.12.2.2. SoC Specific Configuration¶
All SoC specific configurations (eg: SPI module registers base address, interrupt configurations, etc.) can be set using SPI_socSetInitCfg() SoC driver API before calling any SPI driver APIs. The default SoC specific configurations can be retrieved using SPI_socGetInitCfg() SoC driver API. Use the APIs OSPI_socSetInitCfg and OSPI_socGetInitCfg for changing the SoC specific configurations for OSPI.
5.12.2.3. SPI Configuration Structure¶
The SPI_soc.c file binds driver with hardware attributes on the board through SPI_config[] structure. This structure must be provided to the SPI driver. It must be initialized before the SPI_init() function is called and cannot be changed afterwards.
Driver requires common SPI_config[] to configure hardware attributes of MCSPI and QSPI/OSPI peripherals on SOC and board. First all MCSPI related hardware attributes is defined followed by QSPI/OSPI hardware attributes. Application will need to include appropriate offset to instance while invoking SPI_open() API..
For details about individual fields of this library structure, see the PDK doxygen documentation
5.12.3. APIs¶
API Reference for application:
#include <ti/drv/spi/SPI.h>
SPI IP V1 driver also supports multi-channel API’s:
#include <ti/drv/spi/MCSPI.h>
Description
5.12.3.1. Open SPI¶
...
Board_init(boardCfg);
...
SPI_socGetInitCfg(SPI_MCSPI_DOMAIN_MCU, peripheralNum, &spi_cfg);
...
SPI_socSetInitCfg(SPI_MCSPI_DOMAIN_MCU, peripheralNum, &spi_cfg);
SPI_Params_init(&spiParams);
spiParams.transferMode = SPI_MODE_BLOCKING;
spiParams.transferCallbackFxn = NULL;
handle = SPI_open(SPI_MCSPI_DOMAIN_MCU, peripheralNum, &spiParams);
Use below sequence for opening the OSPI instance:
...
OSPI_Params ospiParams;
Board_init(boardCfg);
...
OSPI_socGetInitCfg(SPI_OSPI_DOMAIN_MCU, peripheralNum, &spi_cfg);
...
OSPI_socSetInitCfg(SPI_OSPI_DOMAIN_MCU, peripheralNum, &spi_cfg);
OSPI_Params_init(&ospiParams);
ospiParams.transferMode = OSPI_MODE_BLOCKING;
ospiParams.transferCallbackFxn = NULL;
handle = OSPI_open(SPI_OSPI_DOMAIN_MCU, peripheralNum, &ospiParams);
SPI IP V1 driver also supports multi-channel open API’s:
...
Board_init(boardCfg);
...
MCSPI_Params_init(&spiParams);
spiParams.transferMode = SPI_MODE_BLOCKING;
spiParams.transferCallbackFxn = NULL;
handle = MCSPI_open(SPI_MCSPI_DOMAIN_MCU, peripheralNum, channel, &spiParams);
At this point SPI driver is ready for data transfer in blocking mode on specific instance identified by handle. Pseudo/Sample code for SPI read/write transaction is included below. Refer example for additional details
...
spiTransaction.count = n; /* Transfer Length */
spiTransaction. txBuf = transmitBuffer; /* Buffer to be written */
spiTransaction.rxBuf = NULL; /* Buffer holding the received data */
transferOK = SPI_transfer(spi, &spiTransaction); /* Perform SPI transfer */
if (!transferOK) {
/* SPI transaction failed */
}
Use below sequence for initiating the transfer with OSPI:
...
OSPI_Transaction ospiTransaction;
ospiTransaction.count = n; /* Transfer Length */
ospiTransaction.txBuf = transmitBuffer; /* Buffer to be written */
ospiTransaction.rxBuf = NULL; /* Buffer holding the received data */
transferOK = OSPI_transfer(ospi, &ospiTransaction); /* Perform OSPI transfer */
if (!transferOK) {
/* OSPI transaction failed */
}
SPI IP V1 driver also supports multi-channel transfer API’s:
...
spiTransaction.count = n; /* Transfer Length */
spiTransaction. txBuf = transmitBuffer; /* Buffer to be written */
spiTransaction.rxBuf = NULL; /* Buffer holding the received data */
transferOK = MCSPI_transfer(spi, &spiTransaction); /* Perform SPI transfer */
if (!transferOK) {
/* SPI transaction failed */
}
Note
SPI_open API supports configuration of data word length in the SPI_Params. Currently IP V1 driver supports 8/16/32-bit word length. 8/16-bit word length.
5.12.4. Examples¶
5.12.4.1. OSPI¶
Name | Description | Expected Results | SoC Supported | Build Type |
---|---|---|---|---|
OSPI_TestApplication | Driver unit test application to validate features and interfaces for OSPI driver | Following prints on console expected: Pass criteria: All tests have passed. | j721e
j7200
j721s2
j784s4
|
makefile |
5.12.4.2. MCSPI¶
Name | Description | Additional EVM Configuration | Expected Results | SoC Supported | Build Type |
---|---|---|---|---|---|
MCSPI_slavemode example application | Application demonstrates slave recieve and transmit features of McSPI. Application use case requires two cores. One acts as Master and Another as slave. connections information and addtional details are as follows. Note: Run the slave mode test and then master mode test for proper execution of the test. |
Core usage: J721E EVM:
MCU2_0 (master) ====== MCU2_1(slave)
J7200 EVM:
MCU2_0 (master) ====== MCU2_1(slave)
J721S2 EVM:
MCU2_0 (master) ====== MCU2_1(slave)
J784S4 EVM:
MCU2_0 (master) ====== MCU2_1(slave)
|
On
slave Core
console:
Starting SPI
Slave test.
All tests
have passed.
On Master
Core console:
Starting SPI
Master test
All tests
have passed.
|
j721e
j7200
j721s2
j784s4
|
makefile |
5.12.5. OSPI Driver Configuration to support QSPI flash¶
If the board has a QSPI flash, the PDK driver needs to be updated to support the QSPI flash:
- Board QSPI Flash Instance Configuration in board_cfg.h
#define BOARD_QSPI_NOR_INSTANCE <OSPI instance connected to QSPI flash>
- SPI SoC Driver Configurations:
...
OSPI_v0_HwAttrs ospi_cfg;
SPI_init();
OSPI_socGetInitCfg(SPI_OSPI_DOMAIN_MCU, BOARD_QSPI_NOR_INSTANCE, &ospi_cfg);
ospi_cfg.xferLines = OSPI_XFER_LINES_QUAD;
ospi_cfg.pageSize = <QSPI flash page size>;
ospi_cfg.devDelays[0] = <QSPI device delay>;
ospi_cfg.devDelays[1] = <QSPI device delay>;
ospi_cfg.devDelays[2] = <QSPI device delay>;
ospi_cfg.devDelays[3] = <QSPI device delay>;
ospi_cfg.rdDataCapDelay = <QSPI read capture delay>;
OSPI_socSetInitCfg(SPI_OSPI_DOMAIN_MCU, BOARD_OSPI_NOR_INSTANCE, &ospi_cfg);
5.12.6. Support for Benchmark Testing¶
Name | Description | Expected Results | SOC/Core Suppported | Build Type |
---|---|---|---|---|
OSPI flash Test App | Test application used for performance benchmarking | Test application will print on the UART console: Board_flashWrite ### bytes at transfer rate #### Kbps Board_flashRead ### bytes at transfer rate #### Mbps Board_flashWrite CPU Load %## Board_flashRead CPU Load %## |
j721e/mcux_0 j721e/mcux_1 j7200/mcux_0 j7200/mcux_1 j721s2/mcux_0 j721s2/mcux_1 j784s4/mcux_0 j784s4/mcux_1 | make |
Note
- Data transfer between DDR and OSPI flash memory, performance measurement does not include time to invalidate/write back cache
- GTC counter (200MHz) used for throughput measurement on A53, and PMU cycle counter (400MHz) on R5
- sysbios load moduel used for load measurement
- Pipeline PHY enabled, DDR mode enabled in DAC mode
- Pipeline PHY disabled, DDR mode disabled in INDAC mode with ospi clock divider of 32
- Read/write transfer size of 1M bytes
- Write transfer size 1M bytes with DMA chunk size of 16 bytes in DAC DMA mode