9.4. FAQ - Supported Cores by example applications¶
9.4.1. Introduction¶
PDK provides multiple example applications that demonstrate use of driver/module. The list below details binaries and compute cores that its expected to be hosted on.
Note
Note that these tables are generated based on last test cycle and all bins will not be tested on all revisions of the silicon, in every test cycle.
Binary Name | To be hosted on compute Core |
---|---|
freertos_test_task_switch | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1,c7x_1,c7x_2 |
freertos_test_ut | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1,c7x_1,c7x_2 |
OSAL_TestApp_freertos | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1,c7x_1,c7x_2 |
OSAL_Baremetal_TestApp | mcu1_0,mcu2_0,mcu3_0 |
sciclient_ccs_init | mcu1_0 |
sciserver_testapp_freertos | mcu1_0 |
sciclient_unit_testapp_freertos | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1 |
ex02_bios_multicore_echo_test_freertos | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1,c7x_1,c7x_2 |
ex02_bios_multicore_echo_testb_freertos | mcu1_0 |
ipc_echo_testb_freertos (DM) | mcu1_0 |
ipc_echo_test_freertos (With Linux) | mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1,c7x_1,c7x_2 |
UART_TestApp_freertos | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1,c7x_1,c7x_2 |
UART_Baremetal_freertos | mcu1_0,mcu2_0,mcu3_0 |
UART_DMA_TestApp_freertos | mcu2_0,mcu2_1,mcu3_0,mcu3_1 |
udma_memcpy_testapp_freertos | mcu1_0, mcu2_0, mcu2_1, mcu3_0, mcu3_1, c7x_1, c7x_2 |
udma_baremetal_memcpy_testapp | mpu1_0, mcu1_0, mcu2_0 |
udma_dru_testapp_freertos | mcu2_0, c7x_1, c7x_2 |
udma_dru_direct_tr_testapp_freertos | mcu2_0, c7x_1, c7x_2 |
udma_sw_trigger_testapp_freertos | mcu1_0 |
udma_chaining_testapp_freertos | mcu1_0 |
udma_crc_testapp_freertos | mcu1_0 |
udma_adc_testapp_freertos | mcu1_0 |
udma_unit_testapp | mcu1_0,mcu2_0,mcu2_1,mcu3_0,mcu3_1 |
OSPI_Baremetal_Flash_TestApp | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1 |
OSPI_Flash_TestApp_freertos | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_1 |
OSPI_Baremetal_Flash_Dma_TestApp | mcu1_0,mcu2_0,mcu2_1,mcu3_0,mcu3_1 |
OSPI_Flash_Dma_TestApp_freertos | mcu1_0,mcu2_0,mcu2_1,mcu3_0,mcu3_1 |
MCSPI_Baremetal_Master_TestApp | mcu1_1 |
MCSPI_Baremetal_Slave_TestApp | mpu1_0 |
MCSPI_Master_TestApp_tirtos | mcu1_0 |
MMCSD_Regression_TestApp_freertos | mcu1_0, mcu2_0, mcu2_1, mcu3_0, mcu3_1 |
MMCSD_EMMC_Baremetal_Regression_TestApp | mcu1_0, mpu1_0 |
MMCSD_Baremetal_DMA_TestApp | mcu1_0 |
GPIO_LedBlink_TestApp_freertos | mcu1_0,mcu1_1,mcu2_0,mcu2_1 |
GPIO_Baremetal_LedBlink_TestApp | mpu1_0,mcu1_0,mcu1_1,mcu2_0,mcu2_1 |
vhwa_sde_testapp_freertos | mcu2_1 |
vhwa_dof_testapp_freertos | mcu2_1 |
vhwa_msc_testapp_freertos | mcu2_0 |
vhwa_ldc_testapp_freertos | mcu2_0 |
vhwa_nf_testapp_freertos | mcu2_0 |
vhwa_viss_testapp_freertos | mcu2_0 |
csitx_transmit_testapp_freertos | mcu2_0 |
csirx_capture_testapp_freertos | mcu2_0 |
dss_display_testapp_freertos | mcu2_0 |
csl_crc_cputest_app | mpu1_0 |
csl_vtm_pvt_sensor_maxt | mcu1_0 |
csl_vtm_pvt_sensor_read | mcu1_0 |
csl_vtm_pvt_sensor_temp_alert | mcu1_0 |
csl_spinlock_test_app | mcu1_0, mcu2_1, mpu1_0 |
csl_esm_clk_loss_test_app | mcu1_0 |
csl_esm_baremetal_test_app | mcu1_0 |
csl_dmTimer_baremetal_test_app | mcu1_0 |
csl_dcc_singleshotmode_app | mcu1_0 |
csl_mcan_evm_loopback_app | mcu1_0, mcu2_1 |
csl_uart_test_app | mcu1_0, mpu1_0 |
csl_ospi_flash_app | mcu1_0 |
csl_vim_baremetal_test_app | mcu1_0,mcu1_1 |
csl_ecc_testapp | mcu1_0 |
board_diag_mem | mpu1_0, mcu1_0 |
board_diag_eeprom | mpu1_0, mcu1_0 |
board_diag_uart | mpu1_0, mcu1_0 |
board_diag_mmcsd | mpu1_0, mcu1_0 |
board_diag_emmc | mpu1_0, mcu1_0 |
board_diag_norflash | mpu1_0, mcu1_0 |
board_diag_temperature | mpu1_0, mcu1_0 |
board_diag_extRtc | mpu1_0, mcu1_0 |
board_diag_led | mpu1_0, mcu1_0 |
board_diag_automationHeader | mpu1_0, mcu1_0 |
Binary Name | To be hosted on compute Core |
---|---|
ipc_rtos_echo_test | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0,c7x_1,c7x_2 |
OSAL_TestApp | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0,c7x_1,c7x_2 |
OSPI_Flash_TestApp | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0 |
safertos_test_task_switch | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0,c7x_1,c7x_2 |
sciclient_rtos_app | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0,c7x_1,c7x_2 |
safertos_test_ut | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0,c7x_1,c7x_2 |
sciclient_unit_testapp | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0,c7x_1,c7x_2 |
UART_TestApp | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0,c7x_1,c7x_2 |
udma_memcpy_testapp | mcu1_0,mcu1_1,mcu2_0,mcu2_1,mcu3_0,mcu3_0,c7x_1,c7x_2 |
vhwa_dof_testapp | mcu2_1 |
vhwa_msc_testapp | mcu2_0 |
vhwa_sde_testapp | mcu2_1 |
vhwa_viss_testapp | mcu2_0 |