3.11. MTOG Safety Example¶
3.11.1. Introduction¶
This example demonstrates the usage of the MTOG module. The example shows how to listen for MTOG error events using the ESM, and also forcing an error in order to demonstrate application notification of a timeout event.
The example demonstrates:
Setting a timeout for MTOG instance
Error injection for an MTOG instance
Error event detection for a timeout event
3.11.2. Use Cases¶
Use Case
Description
ESM
UC-1
The MTOG is programmed with a timeout that is small enough to trigger a timeout event on any access. Error event is triggered and application is notified of the event.
MAIN_ESM0
3.11.3. Example Details¶
The example should be loaded to the hardware using the Secondary Boot Loader (SBL) from the SDK.
Example Name |
Location |
Build Command |
|---|---|---|
mtog_app |
[sdl_install_dir]/examples/mtog/ |
make mtog_app PROFILE=release |
3.11.4. Expected Output¶
MTOG Safety Example
sdlAppEsmSetupCommon...Done
sdlAppEsmSetupCommon...Done
sdlAppEsmSetup...Done
Starting MTOG test on MAIN MTOG0, index 0...
sdlAppEsmConfig...Done
MTOG Reset done
sdlAppEsmDisable...Done Delta MTOG prep time in micro secs 27053
Delta MTOG execution time in micro secs 18036
Delta MTOG restore time in micro secs 28047
MTOG complete for MAIN MTOG0
MTOG Saftey Example passed.
mtog_main.c:190:test_sdl_mtog_test_app:PASS
-----------------------
1 Tests 0 Failures 0 Ignored
OK