![]() |
SDL API Guide for J7200
|
Sub Modules | |
| Built-In Test (PBIST) | |
| CPU Compare Module(CCM) | |
| Dual Clock Comparator(DCC) | |
| Error Correction Code(ECC) | |
| Error Signaling Module (ESM) | |
| Logical Built-In Test (LBIST) | |
| MSMC API | |
| Master Timeout Gasket(MTOG) | |
| Memory Cyclic Redundancy check(MCRC) | |
| This file contains the prototypes of the APIs present in the device abstraction layer file of MCRC. This also contains some related macros. | |
| Power OK(POK) | |
| RAT API | |
| ROM_CHECKSUM API | |
| Real Time Interrupt(RTI) | |
| SDL MPU API | |
| Timeout Gasket(TOG) | |
| Voltage and Thermal Monitor(VTM) | |