2.1. Release Notes - 01_00_00¶
2.1.1. Introduction¶
This release notes provides important information that will assist you in using the SDL software package for the J7200 family of devices. This document provides the product information and known issues that are specific to the SDL software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility
2.1.2. What’s New¶
SDL Support for the following modules is provided:
R5F PMU, MPU, RAT and VIM
ESM
PBIST
LBIST
POK
VTM
TOG
ECC
RTI
R5F CCM
DCC
MCRC
Safety Examples for the following modules:
ESM
POK
VTM
TOG
DCC
RTI
ECC
BIST
2.1.3. Supported Devices¶
Supported Devices |
---|
J7200 / DRA821 |
2.1.4. Fixed Issues¶
None - This is the first release.
2.1.5. Known Issues and Limitations¶
Issue Id |
Description |
Workaround |
---|---|---|
PROC_SDL-3343 |
SDL ECC error injection test fails for certain endpoint of certain IPs (MCU R5F 0/1 RAM ID 32/33, VC_MAIN_RC_ECC_AGGR4 RAM ID 71, PSRAM2KECC0_ECC_AGGR, RAM ID 0, VCL_MAIN_INFRA_ECC_AGGR0_1 RAM ID 83) also (CPSW, OSPI, HPB) |
None - This issue is under investigation. Root cause may be incorrect metadata and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. Due to this, the ECC error inject functionality for the mentioned IPs and endpoints is not usable in this release. |
PROC_SDL-3351 |
Illegal boundary crossing test for R5F RAT module fails. |
None - This issue is under investigation. |
PROC_SDL-3375 |
Testing gaps for DRU/UTC ECC requirements. Test cases need to be identified. |
None - Metadata for all ECC instances is available. However, which ECC aggregator is associated with these IPs is not known at release time. Once confirmed, no code changes will be needed to resolve this issue. Only traceability will be updated. |
2.1.6. Migration Information¶
None
2.1.7. Tool Chain Information¶
Component |
Version |
---|---|
TI ARM R5F Clang Compiler tools |
1.3.0.LTS |