3.11. MTOG Safety Example

3.11.1. Introduction

This example demonstrates the usage of the MTOG module. The example shows how to listen for MTOG error events using the ESM, and also forcing an error in order to demonstrate application notification of a timeout event.

The example demonstrates:

  • Setting a timeout for MTOG instance

  • Error injection for an MTOG instance

  • Error event detection for a timeout event

3.11.2. Use Cases

Use Case

Description

ESM

UC-1

The MTOG is programmed with a timeout that is small enough to trigger a timeout event on any access. Error event is triggered and application is notified of the event.

MAIN_ESM0

3.11.3. Example Details

The example should be loaded to the hardware using the Secondary Boot Loader (SBL) from the SDK.

Example Name

Location

Build Command

mtog_app

[sdl_install_dir]/examples/mtog/

make mtog_app PROFILE=release

3.11.4. Expected Output

MTOG Safety Example

 sdlAppEsmSetupCommon...Done
 sdlAppEsmSetupCommon...Done
 sdlAppEsmSetup...Done
 Starting MTOG test on MAIN MTOG0, index 0...
 sdlAppEsmConfig...Done
 MTOG Reset done
 sdlAppEsmDisable...Done  Delta MTOG prep time in micro secs 27053
  Delta MTOG execution time in micro secs 18036
  Delta MTOG restore time in micro secs 28047
  MTOG complete for MAIN MTOG0

 MTOG Saftey Example passed.
mtog_main.c:190:test_sdl_mtog_test_app:PASS

-----------------------
1 Tests 0 Failures 0 Ignored
OK

3.11.5. Reference

MTOG User Guide