![]() |
SDL API Guide for J7200
|
The Digital Watchdog Timer(DWT) generates reset after a programmable period, if not serviced within that period. In DWT, time-out boundary is configurable. In DWWD, along with configurable time-out boundary, the start time boundary is also configurable. The DWWD can generate Reset or Interrupt, if not serviced within window(Open Window) defined by start time and time-out boundary. Also the DWWD can generate Reset or Interrupt if serviced outside Open Window (within Closed Window). Generation of Reset or Interrupt depends on the DWWD Reaction configuration.
Sub Modules | |
RTI Data Structures | |
RTI Enumerated Types | |
RTI Functions | |