2. Getting Started

2.1. Build from Source

Refer below table to get started with topic of your interest.

Topic

Documentation Links

Gateway

See ethernet firmware [LINK]

See gateway demos [LINK]

Integrated MCU

See MCUSW [LINK]

RTOS Device Drivers

See PDK [LINK]

2.2. Running Out of the Box Demos

Out of the Box Demos refers to prebuilt linux filesystem and boot partition with demo binaries and firmware preintegrated. It is downloadable as a tar ball from the SDK release page and can be extracted to an SD card and loaded on the board via a simple script without the need to download the source package or build anything.

J7200 does not yet have any out of box demos.