72 #define UDMA_TR_TYPE_0 (CSL_UDMAP_TR_FLAGS_TYPE_1D_DATA_MOVE)
73 #define UDMA_TR_TYPE_1 (CSL_UDMAP_TR_FLAGS_TYPE_2D_DATA_MOVE)
74 #define UDMA_TR_TYPE_2 (CSL_UDMAP_TR_FLAGS_TYPE_3D_DATA_MOVE)
75 #define UDMA_TR_TYPE_3 (CSL_UDMAP_TR_FLAGS_TYPE_4D_DATA_MOVE)
76 #define UDMA_TR_TYPE_4 (CSL_UDMAP_TR_FLAGS_TYPE_4D_DATA_MOVE_FORMATTING)
77 #define UDMA_TR_TYPE_5 (CSL_UDMAP_TR_FLAGS_TYPE_4D_CACHE_WARM)
78 #define UDMA_TR_TYPE_8 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE)
79 #define UDMA_TR_TYPE_9 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE_REPACKING)
80 #define UDMA_TR_TYPE_10 (CSL_UDMAP_TR_FLAGS_TYPE_2D_BLOCK_MOVE)
81 #define UDMA_TR_TYPE_11 (CSL_UDMAP_TR_FLAGS_TYPE_2D_BLOCK_MOVE_REPACKING)
82 #define UDMA_TR_TYPE_15 (CSL_UDMAP_TR_FLAGS_TYPE_4D_BLOCK_MOVE_REPACKING_INDIRECTION)
94 #define UDMA_GET_TRPD_TR15_SIZE(n) (UDMA_ALIGN_SIZE(sizeof(CSL_UdmapTR15) + ((n) * (sizeof(CSL_UdmapTR15) + 4U))))
99 #define UDMA_TR1_OFFSET (64U)
179 uint32_t descType = CSL_UDMAP_CPPI5_PD_DESCINFO_DTYPE_VAL_TR;
183 CSL_udmapCppi5SetDescType(pTrpd, descType);
184 CSL_udmapCppi5TrSetReload((CSL_UdmapCppi5TRPD*)pTrpd, 0U, 0U);
185 CSL_udmapCppi5SetPktLen(pTrpd, descType, trCnt);
187 CSL_udmapCppi5SetSrcTag(pTrpd, 0x0000);
188 CSL_udmapCppi5SetDstTag(pTrpd, 0x0000);
189 CSL_udmapCppi5TrSetEntryStride((CSL_UdmapCppi5TRPD*)pTrpd, trSizeEncoded);
190 CSL_udmapCppi5SetReturnPolicy(
193 CSL_UDMAP_CPPI5_PD_PKTINFO2_RETPOLICY_VAL_ENTIRE_PKT,
194 CSL_UDMAP_CPPI5_PD_PKTINFO2_EARLYRET_VAL_NO,
195 CSL_UDMAP_CPPI5_PD_PKTINFO2_RETPUSHPOLICY_VAL_TO_TAIL,
#define UDMA_DEFAULT_FLOW_ID
Default flow ID.
Definition: udma_flow.h:66
static void UdmaUtils_makeTrpd(void *pTrpd, uint32_t trType, uint32_t trCnt, uint32_t cqRingNum)
UDMA utility API to make TRPD. Other TRPD make APIs should be called only after this API.
Definition: udma_utils.h:174
uint32_t UdmaUtils_getTrSizeEncoded(uint32_t trType)
Returns the size of TR (encoded) based on the type.
uint32_t UdmaUtils_getTrSizeBytes(uint32_t trType)
Returns the size of TR in bytes based on the type.
CSL_UdmapTR1 * UdmaUtils_getTrpdTr1Pointer(uint8_t *trpdMem, uint32_t trIndex)
Returns the TR1 pointer in the TRPD memory based on the index.
uint32_t UdmaUtils_getRingMemSize(uint8_t mode, uint32_t elemCnt, uint8_t elemSize)
UDMA get ring size utility API.