4.1. Release notes - 10_01_00¶
4.1.1. Documentation¶
The documentation included with the PSDK QNX J784S4 is specific to the PSDK QNX J784S4 package.
PSDK RTOS J784S4 package documentation (PSDK RTOS Components) must also be referenced, for full understanding of PSDK QNX J784S4 support.
4.1.2. PSDK QNX J784S4 Features¶
Note
Reference PSDK RTOS J784S4 package documentation (LINK) for an extensive list of new and current features supported by PSDK QNX + PSDK RTOS. This section lists only the features that are PSDK QNX J784S4 specific.
For features & drivers enabled by the QNX BSP, please refer to BSP Documentation or contact QNX.
The release is tested on Ubuntu (x86_64) 22.04 systems and may not work on earlier or later Ubuntu systems.
If using low-mem codec carveout prior to this release, please adjust your startup carveouts accrdingly, as the TI configuration no longer provides this by default
4.1.2.1. Enabled in this Release¶
Features enabled in this release, specific to PSDK QNX J784S4 addon package are:
Support for QNX SDP 8.0
As part of SDP 8.0 migration, io-sock driver from QNX is the supported networking stack for this platform.
Freed up unused low-mem codec careveout (256MB) in j784s4-evm-ti.build file
For additional new updates, please refer PSDK RTOS package documentation (PSDK RTOS Components).
4.1.2.2. Enabled in Previous Releases¶
Features enabled in previous release, specific to PSDK QNX J784S4 addon package are:
VPU video codec updates
Empirical values for internal and external buffers used for Codec published.
Various encode and decode fps rates published.
Resource manager support for VPU video encoder
Resource manager support for VPU video decoder
Multicore codec support.
Codec IO-buffer and Internal buffer management using SharedMemoryAllocator.
Supports usage of DDR high-mem (>4G range). Default base address is “0x8 C000 0000” with a total of 768MB.
OMX IL Component support for VPU video encoder and File-based OMX encoder test application (H.264 & HEVC)
Configurable GOP Preset support. Can configure combinations of I and P frames
Supports logging at different levels
Supports a multi-threaded implementation
Encoder multichannel support upto 8x1080p streams
Encoder supports performance upto 1x1080p at 60fps and 2x1080p at 30fps
OMX IL Component support for VPU video decoder and File-based OMX decoder test application (H.264 & HEVC)
Support for YUV 420 and pseudo-YUV 422 output formats.
Supports zero-copy buffer passing between application and codec
Supports I, P and B frame decoding
Supports decode of stream headers in advance
Supports logging at different levels
Supports a multi-threaded implementation
HW Watchdog for Decoder
Decoder to recovery from SW stream errors
Decoder supports deblocking filter
Support for block-level spatial & temporal error concealment
Support for user input to determine number of non-linear frame buffers
VPU codec (encoder and decoder) with test app
HEVC & H.264 4K Encode support with file-to-file encode test app
HEVC & H.264 4K Decode support with file-to-file decode test app
Multi-instance HEVC/H.264 Encode & Decode support with multi-inst test app
OMX IL Component support for VPU video encode & decode (H.264 & HEVC)
Decode/Encode: Support for 2x HW VPU instances for Video Encode / Decode
Decode/Encode: Supports Interrupt mode for VPU codec
Decode/Encode: Supports 8 channel D1@30fps Encode + 8 channel D1@30fps Decode
Encode: Supports Rate control - VBR and CBR
Encode: Supports CBR (e.g., for Video Conferencing), 2-10 Mbps
Decode: Performance profiler added for VPU decode
Decode: Publish Codec Capabilities through API
Bug fixes
Sciclient random ACK failure fixed.
UDMA Resource Manager fixed the duplicate UDMA flow-id allocation
Running iperf with parallel instance of cpsw2g and cpsw9g
The ipc_test failing to ping ipc echo testb DM image
The tiudma-mgr cannot be restarted after being slayed
The udma_memcpy_test hangs forever in case of failure
CPSW2G direct ethernet cable connection
Decode: Fixed junk frames at the end for streams greater than 1080p
Decode/Encode: Multi-instance decode/encode failure fixed
Decode: OMX decoder fails to decode H.264 Level5 bitstreams of long play length
Decode: VPU fails to decode high-bitrate (>100 Mbps) 4K resolution videos
Decode: OMX decoder fails to decode 2x 4K HEVC/H264 bitstreams due to out-of-memory
Decode: OMX decode application does not check for num input bufs being exactly 2
Decode: OMX decode of 4x H.264 1080p bitstreams produces incorrect output frames
UDMA driver refactor to enable concurrent access of udma resources
Added test capability to support larger memcpy for UDMA
IPC driver returns incorrect return code during a timeout
Remove dependency on bootloader to set the MMCSD clocks
Added support to allocate UDMA proxy per process
For additional new updates, please refer PSDK RTOS package documentation (PSDK RTOS Components).
4.1.2.3. Change Requests¶
The following Change requests have been made for this release.
VPU changes
Encoder: Descope configurable block sizes due to lack of HW support
Decoder: Move non-fatal error code support to 10.1 release
Re-evaluate safety requirement for TI’s reference shared memory allocator
4.1.2.4. Errata¶
Please refer release note in the PSDK RTOS J784S4 package documentation (PSDK RTOS Components) for the complete errata list.
4.1.3. Software Dependencies¶
4.1.3.1. QNX Dependency¶
Note
The PSDK QNX addon package is dependent on installations from QNX Software Center. The below QNX packages were used for PSDK QNX 10_01_00 build and verification.
4.1. QNX SDP 8.0¶
QNX SDP 800 Package |
Build ID |
Package ID |
Package Version |
|---|---|---|---|
QNX® Software Development Platform 8.0 |
141 |
com.qnx.qnx800 |
(Validated against this version contact QNX for latest) |
QNX® SDP 8.0 Screen Board Support J784S4 (with Debug Symbols) |
123 |
com.qnx.qnx800.target.screen.board.j784s4 |
4.0.1.00123T202404231650L |
QNX® SDP 8.0 BSP for Texas Instruments Jacinto 7 J784S4 Evaluation Modules |
73 |
com.qnx.qnx800.bsp.hw.ti_j784s4_evm |
0.0.1.00073T202405131122L |
QNX® SDP 8.0 Networking - io-sock |
135 |
com.qnx.qnx800.target.net.iosock |
0.0.1.00135T202311191043L |
4.1.3.2. PSDK RTOS Dependency¶
The PSDK QNX package is an addon package to the PSDK RTOS release, as such the PSDK RTOS is required.
4.1.4. Device Support and Validation Information¶
SoC |
Build Host (OS) |
Run Target (OS) |
Test Platform |
|---|---|---|---|
J784S4 |
x86_64 (Linux Ubuntu 22.04) |
R5F & C7x running TI-RTOS A72 running QNX |
TI EVM with daughter cards |
Note
Refer EVM Setup for J784S4 for more details on the TI EVM support.
4.1.5. Open Defects¶
Below table lists all the current open defects:
ID |
Head Line |
|---|---|
QNX: J721S2 & J784S4 IPC round trip time is greater than expected range |
|
VPU: OMX decoder fails to decode H.264 mixed resolution 1080p/720p video |
|
VPU: QNX Encoder Performance - 4x 1080p60 not met. At 47fps now |
|
Virtual client: io-pkt: Fix memory leak during CPSW recovery |
|
Address Compiler Warning -Wno-address-of-packed-member |
|
SDK to evaluate and remove short_enums compiler flag across modules |
4.1.6. Closed Issues¶
Below table lists all the defects closed from previous releases:
ID |
Head Line |
|---|---|
CPSW5G/9G: Destroying interface freezes prompt |
|
SafeRTOS: IPC echo test fails to ping mcu cores |
4.1.7. Known Issues¶
A list of key known issues with the PSDK QNX release is provided below.
Note
Refer to individual PSDK RTOS Components release notes for known issues in each component
Index |
Module |
Description |
|---|---|---|
1 |
QNX UDMA RM |
UDMA resource manager may not free UDMA resources when client exits unexpectedly. |
2 |
QNX Networking (io-sock) |
Issues have been seen trying to run io-sock with revision com.qnx.qnx800.target.net.iosock/0.0.2.00417T202407041502L. Please use the specified revision mentioned above. Further support should be directed to QNX. |
4.1.8. Additional Reports¶
For additional reports like test report, traceability refer PSDK RTOS Additional Reports